![]() |
SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.55
Simplifies the implementation of Internet connectivity
|
Networking related commands and configuration. More...
Functions | |
_i32 | sl_NetUtilSet (const _u16 Option, const _u32 ObjID, const _u8 *pValues, const _u16 ValueLen) |
Function for setting configurations of utilities. More... | |
_i16 | sl_NetUtilGet (const _u16 Option, const _u32 ObjID, _u8 *pValues, _u16 *pValueLen) |
Function for getting configurations of utilities. More... | |
_i16 | sl_NetUtilCmd (const _u16 Cmd, const _u8 *pAttrib, const _u16 AttribLen, const _u8 *pInputValues, const _u16 InputLen, _u8 *pOutputValues, _u16 *pOutputLen) |
Function for performing utilities-related commands. More... | |
Networking related commands and configuration.
_i16 sl_NetUtilCmd | ( | const _u16 | Cmd, |
const _u8 * | pAttrib, | ||
const _u16 | AttribLen, | ||
const _u8 * | pInputValues, | ||
const _u16 | InputLen, | ||
_u8 * | pOutputValues, | ||
_u16 * | pOutputLen | ||
) |
Function for performing utilities-related commands.
[in] | Cmd | Identifier of the specific Command to perform
|
[in] | pAttrib | Pointer to the buffer holding the Attribute values |
[in] | AttribLen | Length of the Attribute-values |
[in] | pInputValues | Pointer to the buffer holding the input-value |
[in] | InputLen | Length of the input-value |
[out] | pOutputValues | Pointer to the buffer that the application allocates, and will hold the received data. |
[in,out] | pOutputLen | Length of the output-value On input - provides the length of the buffer that the application allocates, and will hold the output On output - provides the actual length of the received output-values |
- SL_NETUTIL_CMD_ARP_LOOKUP, (Mapping MAC address to IPv4 or IPv6 address), CC3235S/SF devices only:
_i16 sl_NetUtilGet | ( | const _u16 | Option, |
const _u32 | ObjID, | ||
_u8 * | pValues, | ||
_u16 * | pValueLen | ||
) |
Function for getting configurations of utilities.
[in] | Option | Identifier of the specific "get" operation to perform
|
[in] | ObjID | ID of the relevant object that this set operation will be performed on |
[in,out] | pValueLen | Pointer to the length of the value parameter On input - provides the length of the buffer that the application allocates, and will hold the output On output - provides the actual length of the received data |
[out] | pValues | Pointer to the buffer that the application allocates, and will hold the received data. |
Definition at line 74 of file netutil.c.
_i32 sl_NetUtilSet | ( | const _u16 | Option, |
const _u32 | ObjID, | ||
const _u8 * | pValues, | ||
const _u16 | ValueLen | ||
) |
Function for setting configurations of utilities.
[in] | Option | Identifier of the specific "set" operation to perform |
[in] | ObjID | ID of the relevant object that this set operation will be performed on |
[in] | ValueLen | Length of the value parameter |
[in] | pValues | Pointer to the buffer holding the configurations values |
struct _SlNetUtilCmdData_t |
struct SlNetUtilCryptoEcCustomCurveParam_t |
union SlNetUtilCryptoEcCurveParams_u |
Data Fields | ||
---|---|---|
SlNetUtilCryptoEcCustomCurveParam_t | CustomCurveParams | |
_u8 | NamedCurveParams |
struct SlNetUtilCryptoEcKeyParams_t |
Data Fields | ||
---|---|---|
SlNetUtilCryptoEcCurveParams_u | CurveParams | |
_u8 | CurveType |
union SlNetUtilCryptoPubKeyParams_u |
Data Fields | ||
---|---|---|
SlNetUtilCryptoEcKeyParams_t | EcParams |
struct SlNetUtilCryptoPubKeyInfo_t |
Data Fields | ||
---|---|---|
_u8 | CertFileNameLen | |
_u8 | KeyAlgo | |
_u8 | KeyFileNameLen | |
SlNetUtilCryptoPubKeyParams_u | KeyParams |
struct SlNetUtilCryptoCmdSignAttrib_t |
struct SlNetUtilCryptoCmdVerifyAttrib_t |
struct SlNetUtilCryptoCmdCreateCertAttrib_t |
struct SlNetUtilCryptoCmdKeyMgnt_t |