UARTCC32XXDMA Object. More...
#include <UARTCC32XXDMA.h>
Data Fields | |
bool | opened |
UART_Mode | readMode |
UART_Mode | writeMode |
unsigned int | readTimeout |
unsigned int | writeTimeout |
UART_Callback | readCallback |
UART_Callback | writeCallback |
UART_ReturnMode | readReturnMode |
UART_DataMode | readDataMode |
UART_DataMode | writeDataMode |
uint32_t | baudRate |
UART_LEN | dataLength |
UART_STOP | stopBits |
UART_PAR | parityType |
UART_Echo | readEcho |
const void * | writeBuf |
size_t | writeCount |
size_t | writeSize |
void * | readBuf |
size_t | readCount |
size_t | readSize |
SemaphoreP_Handle | writeSem |
SemaphoreP_Handle | readSem |
HwiP_Handle | hwiHandle |
ClockP_Handle | txFifoEmptyClk |
Power_NotifyObj | postNotify |
unsigned int | powerMgrId |
PowerCC32XX_ParkState | prevParkTX |
uint16_t | txPin |
PowerCC32XX_ParkState | prevParkRTS |
uint16_t | rtsPin |
UDMACC32XX_Handle | dmaHandle |
UARTCC32XXDMA Object.
The application must not access any member variables of this structure!
bool UARTCC32XXDMA_Object::opened |
UART_Mode UARTCC32XXDMA_Object::readMode |
UART_Mode UARTCC32XXDMA_Object::writeMode |
unsigned int UARTCC32XXDMA_Object::readTimeout |
unsigned int UARTCC32XXDMA_Object::writeTimeout |
UART_Callback UARTCC32XXDMA_Object::readCallback |
UART_Callback UARTCC32XXDMA_Object::writeCallback |
UART_ReturnMode UARTCC32XXDMA_Object::readReturnMode |
UART_DataMode UARTCC32XXDMA_Object::readDataMode |
UART_DataMode UARTCC32XXDMA_Object::writeDataMode |
uint32_t UARTCC32XXDMA_Object::baudRate |
UART_LEN UARTCC32XXDMA_Object::dataLength |
UART_STOP UARTCC32XXDMA_Object::stopBits |
UART_PAR UARTCC32XXDMA_Object::parityType |
UART_Echo UARTCC32XXDMA_Object::readEcho |
const void* UARTCC32XXDMA_Object::writeBuf |
size_t UARTCC32XXDMA_Object::writeCount |
size_t UARTCC32XXDMA_Object::writeSize |
void* UARTCC32XXDMA_Object::readBuf |
size_t UARTCC32XXDMA_Object::readCount |
size_t UARTCC32XXDMA_Object::readSize |
SemaphoreP_Handle UARTCC32XXDMA_Object::writeSem |
SemaphoreP_Handle UARTCC32XXDMA_Object::readSem |
HwiP_Handle UARTCC32XXDMA_Object::hwiHandle |
ClockP_Handle UARTCC32XXDMA_Object::txFifoEmptyClk |
Power_NotifyObj UARTCC32XXDMA_Object::postNotify |
unsigned int UARTCC32XXDMA_Object::powerMgrId |
PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkTX |
uint16_t UARTCC32XXDMA_Object::txPin |
PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkRTS |
uint16_t UARTCC32XXDMA_Object::rtsPin |
UDMACC32XX_Handle UARTCC32XXDMA_Object::dmaHandle |