TimerCC32XX_Object.
More...
#include <TimerCC32XX.h>
TimerCC32XX_Object.
The application must not access any member variables of this structure!
§ hwiHandle
HwiP_Handle TimerCC32XX_Object::hwiHandle |
§ notifyObj
§ timerSem
SemaphoreP_Handle TimerCC32XX_Object::timerSem |
§ callBack
§ mode
§ timer
uint32_t TimerCC32XX_Object::timer |
§ period
uint32_t TimerCC32XX_Object::period |
§ prescaler
uint32_t TimerCC32XX_Object::prescaler |
§ isRunning
bool TimerCC32XX_Object::isRunning |
The documentation for this struct was generated from the following file: