72 #ifndef ti_drivers_sd_SDHostCC32XX__include 73 #define ti_drivers_sd_SDHostCC32XX__include 78 #include <ti/drivers/dpl/HwiP.h> 79 #include <ti/drivers/dpl/SemaphoreP.h> 88 #define SDHostCC32XX_PIN_06_SDCARD_DATA 0x0805 89 #define SDHostCC32XX_PIN_07_SDCARD_CLK 0x0806 90 #define SDHostCC32XX_PIN_08_SDCARD_CMD 0x0807 91 #define SDHostCC32XX_PIN_01_SDCARD_CLK 0x0600 92 #define SDHostCC32XX_PIN_02_SDCARD_CMD 0x0601 93 #define SDHostCC32XX_PIN_64_SDCARD_DATA 0x063f volatile int_fast8_t stat
Definition: SDHostCC32XX.h:189
SemaphoreP_Handle cmdSem
Definition: SDHostCC32XX.h:175
uint32_t clkPin
Definition: SDHostCC32XX.h:156
uint_fast32_t baseAddr
Definition: SDHostCC32XX.h:141
int_fast32_t intPriority
Definition: SDHostCC32XX.h:138
Power_NotifyObj postNotify
Definition: SDHostCC32XX.h:183
bool ping
Definition: SDHostCC32XX.h:193
uint_fast32_t clkRate
Definition: SDHostCC32XX.h:135
SDHostCC32XX Object.
Definition: SDHostCC32XX.h:164
bool dmaPosted
Definition: SDHostCC32XX.h:195
uint32_t dataPin
Definition: SDHostCC32XX.h:150
SD_CardType cardType
Definition: SDHostCC32XX.h:197
uDMA driver implementation for CC32XX.
The definition of a SD function table that contains the required set of functions to control a specif...
Definition: SD.h:285
bool isOpen
Definition: SDHostCC32XX.h:191
UDMACC32XX Global configuration.
Definition: UDMACC32XX.h:125
volatile uint32_t sectorCount
Definition: SDHostCC32XX.h:168
Power manager interface for the CC32XX.
uint32_t cmdPin
Definition: SDHostCC32XX.h:153
Secure Digital (SD) Driver.
unsigned long txChIdx
Definition: SDHostCC32XX.h:147
UDMACC32XX_Handle dmaHandle
Definition: SDHostCC32XX.h:179
volatile uint32_t rca
Definition: SDHostCC32XX.h:166
Power notify object structure.
Definition: Power.h:443
HwiP_Handle hwiHandle
Definition: SDHostCC32XX.h:177
PowerCC32XX_ParkState prevParkCLK
Definition: SDHostCC32XX.h:185
uint16_t clkPin
Definition: SDHostCC32XX.h:187
SD_CardType
SD Card type inserted.
Definition: SD.h:197
volatile uint32_t * buffer
Definition: SDHostCC32XX.h:170
unsigned long rxChIdx
Definition: SDHostCC32XX.h:144
const SD_FxnTable sdHostCC32XX_fxnTable
Definition: SDHostCC32XX.h:133
unsigned int powerMgrId
Definition: SDHostCC32XX.h:181
PowerCC32XX_ParkState
Enumeration of states a pin can be parked in.
Definition: PowerCC32XX.h:385