41 #include <ti/drivers/net/wifi/simplelink.h> 51 _i32 RetVal_stop = -1;
55 _u16 ipConfigSize = 0;
67 if ((SimpleLinkWifiCC32XX_config.Mode != SL_DEVICE_SYSCONFIG_AS_CONFIGURED) && (SimpleLinkWifiCC32XX_config.Mode != Mode))
89 if(SimpleLinkWifiCC32XX_config.Mode != RetVal)
97 if (SimpleLinkWifiCC32XX_config.ConnectionPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
101 SimpleLinkWifiCC32XX_config.ConnectionPolicy,
108 if (SimpleLinkWifiCC32XX_config.ProvisioningStop)
121 if (SimpleLinkWifiCC32XX_config.DeleteAllProfile)
132 if (SimpleLinkWifiCC32XX_config.Ipv4Config != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
134 if (SimpleLinkWifiCC32XX_config.Mode == ROLE_STA)
136 uIPMode = SL_NETCFG_IPV4_STA_ADDR_MODE;
138 else if (SimpleLinkWifiCC32XX_config.Mode == ROLE_AP)
140 uIPMode = SL_NETCFG_IPV4_AP_ADDR_MODE;
142 if (SimpleLinkWifiCC32XX_config.Ipv4Config == SL_NETCFG_ADDR_STATIC)
147 localIpV4.Ip = (_u32)SimpleLinkWifiCC32XX_config.Ipv4;
148 localIpV4.IpMask = (_u32)SimpleLinkWifiCC32XX_config.IpMask;
149 localIpV4.IpGateway = (_u32)SimpleLinkWifiCC32XX_config.IpGateway;
150 localIpV4.IpDnsServer = (_u32)SimpleLinkWifiCC32XX_config.IpDnsServer;
152 else if (SimpleLinkWifiCC32XX_config.Ipv4Config != SL_NETCFG_ADDR_DHCP)
161 RetVal =
sl_NetCfgSet(uIPMode, SimpleLinkWifiCC32XX_config.Ipv4Config, ipConfigSize, (_u8 *)ipV4);
169 if (SimpleLinkWifiCC32XX_config.ScanPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
171 _u32 intervalInSeconds = SimpleLinkWifiCC32XX_config.ScanIntervalInSeconds;
172 ucConfigOpt = SimpleLinkWifiCC32XX_config.ScanPolicy;
173 RetVal =
sl_WlanPolicySet(SL_WLAN_POLICY_SCAN, ucConfigOpt, (_u8 *)&intervalInSeconds,
sizeof(intervalInSeconds));
181 if (SimpleLinkWifiCC32XX_config.PMPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
183 if (SimpleLinkWifiCC32XX_config.PMPolicy != SL_WLAN_LONG_SLEEP_INTERVAL_POLICY)
185 RetVal =
sl_WlanPolicySet(SL_WLAN_POLICY_PM, SimpleLinkWifiCC32XX_config.PMPolicy, NULL,0);
195 PmPolicyParams.MaxSleepTimeMs = SimpleLinkWifiCC32XX_config.MaxSleepTimeMS;
196 RetVal =
sl_WlanPolicySet(SL_WLAN_POLICY_PM, SimpleLinkWifiCC32XX_config.PMPolicy, (_u8*)&PmPolicyParams,
sizeof(PmPolicyParams));
205 if (SimpleLinkWifiCC32XX_config.DHCPServer)
209 dhcpParams.lease_time = SimpleLinkWifiCC32XX_config.LeaseTime;
210 dhcpParams.ipv4_addr_start = (_u32)SimpleLinkWifiCC32XX_config.StartAddress;
211 dhcpParams.ipv4_addr_last = (_u32)SimpleLinkWifiCC32XX_config.LastAddress;
217 RetVal =
sl_NetAppSet(SL_NETAPP_DHCP_SERVER_ID, SL_NETAPP_DHCP_SRV_BASIC_OPT, outLen, (_u8* )&dhcpParams);
222 if (SimpleLinkWifiCC32XX_config.Mode == ROLE_AP)
_i16 sl_WlanSetMode(const _u8 Mode)
Wlan set mode.
_i16 sl_NetAppSet(const _u8 AppId, const _u8 Option, const _u8 OptionLen, const _u8 *pOptionValue)
Setting network application configurations.
_i16 sl_WlanProvisioning(_u8 ProvisioningCmd, _u8 RequestedRoleAfterSuccess, _u16 InactivityTimeoutSec, char *pSmartConfigKey, _u32 Flags)
The simpleLink will switch to the appropriate role according to the provisioning mode requested and w...
_i16 sl_Stop(const _u16 Timeout)
Stop the SimpleLink device.
_i16 sl_WlanPolicySet(const _u8 Type, const _u8 Policy, _u8 *pVal, const _u8 ValLen)
Set policy values.
_i32 sl_WifiConfig()
Configure SimpleLink to default state.
_i16 sl_NetCfgSet(const _u16 ConfigId, const _u16 ConfigOpt, const _u16 ConfigLen, const _u8 *pValues)
Setting network configurations.
_i16 sl_WlanProfileDel(const _i16 Index)
Delete WLAN profile.
_i16 sl_NetAppStart(const _u32 AppBitMap)
Starts a network application.
_i16 sl_NetAppStop(const _u32 AppBitMap)
Stops a network application.
_i16 sl_Start(const void *pIfHdl, _i8 *pDevName, const P_INIT_CALLBACK pInitCallBack)
Start the SimpleLink device.