SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.55
Simplifies the implementation of Internet connectivity
SlSocketAddrIPv4Command_t Struct Reference

Data Fields

_i16 LenOrPadding
 
_u8 Sd
 
_u8 FamilyAndFlags
 
_u16 Port
 
_u16 PaddingOrAddr
 
_u32 Address
 

Detailed Description

Definition at line 824 of file protocol.h.

Field Documentation

§ Address

_u32 Address

Definition at line 831 of file protocol.h.

§ FamilyAndFlags

_u8 FamilyAndFlags

Definition at line 828 of file protocol.h.

§ LenOrPadding

_i16 LenOrPadding

Definition at line 826 of file protocol.h.

§ PaddingOrAddr

_u16 PaddingOrAddr

Definition at line 830 of file protocol.h.

§ Port

_u16 Port

Definition at line 829 of file protocol.h.

§ Sd

_u8 Sd

Definition at line 827 of file protocol.h.


The documentation for this struct was generated from the following file: