Data Fields
CryptoCC32XX_AesAadParams Union Reference

AES Additional Authentication Data Parameters. More...

#include <CryptoCC32XX.h>

Collaboration diagram for CryptoCC32XX_AesAadParams:
Collaboration graph
[legend]

Data Fields

CryptoCC32XX_AesAadInputParams input
 
uint8_t tag [16]
 

Detailed Description

AES Additional Authentication Data Parameters.

This union defines the AES additional authentication parameters used for CryptoCC32XX_AES_GCM and CryptoCC32XX_AES_CCM

Field Documentation

§ input

CryptoCC32XX_AesAadInputParams CryptoCC32XX_AesAadParams::input

an input - additional authentication data

§ tag

uint8_t CryptoCC32XX_AesAadParams::tag[16]

an output - pointer to a 4-word array where the hash tag is written


The documentation for this union was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale