![]() |
SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.54
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | Ip [4] |
_u8 | IpMask [4] |
_u8 | IpGateway [4] |
_u8 | IpDnsServer [4] |
_u8 | IpStart [4] |
_u8 | IpEnd [4] |
Definition at line 735 of file protocol.h.
_u8 Ip[4] |
Definition at line 737 of file protocol.h.
_u8 IpDnsServer[4] |
Definition at line 740 of file protocol.h.
_u8 IpEnd[4] |
Definition at line 742 of file protocol.h.
_u8 IpGateway[4] |
Definition at line 739 of file protocol.h.
_u8 IpMask[4] |
Definition at line 738 of file protocol.h.
_u8 IpStart[4] |
Definition at line 741 of file protocol.h.