SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.46
Simplifies the implementation of Internet connectivity
Device

Controls the behaviour of the CC31xx/CC32xx device (start/stop, events masking and obtaining specific device status) More...

Functions

_i16 sl_Start (const void *pIfHdl, _i8 *pDevName, const P_INIT_CALLBACK pInitCallBack)
 Start the SimpleLink device. More...
 
_i16 sl_Stop (const _u16 Timeout)
 Stop the SimpleLink device. More...
 
_i16 sl_DeviceSet (const _u8 DeviceSetId, const _u8 Option, const _u16 ConfigLen, const _u8 *pValues)
 Setting device configurations. More...
 
_i16 sl_DeviceGet (const _u8 DeviceGetId, _u8 *pOption, _u16 *pConfigLen, _u8 *pValues)
 Internal function for getting device configurations. More...
 
_i16 sl_DeviceEventMaskSet (const _u8 EventClass, const _u32 Mask)
 Set asynchronous event mask. More...
 
_i16 sl_DeviceEventMaskGet (const _u8 EventClass, _u32 *pMask)
 Get current event mask of the device. More...
 
void * sl_Task (void *pEntry)
 The SimpleLink task entry. More...
 
_i16 sl_DeviceUartSetMode (const SlDeviceUartIfParams_t *pUartParams)
 Setting the internal uart mode. More...
 
_i32 sl_WifiConfig ()
 Configure SimpleLink to default state. More...
 

Typedefs

typedef struct SlDeviceFatalNoCmdAck_t SlDeviceFatalCmdTimeout_t
 
typedef void(* P_INIT_CALLBACK) (_u32 Status, SlDeviceInitInfo_t *DeviceInitInfo)
 

Enumerations

enum  SlDeviceEventId_e {
  SL_DEVICE_EVENT_FATAL_DEVICE_ABORT = 1,
  SL_DEVICE_EVENT_FATAL_DRIVER_ABORT,
  SL_DEVICE_EVENT_FATAL_SYNC_LOSS,
  SL_DEVICE_EVENT_FATAL_NO_CMD_ACK,
  SL_DEVICE_EVENT_FATAL_CMD_TIMEOUT,
  SL_DEVICE_EVENT_RESET_REQUEST,
  SL_DEVICE_EVENT_ERROR,
  SL_DEVICE_EVENT_MAX
}
 
enum  SlDeviceSource_e {
  SL_DEVICE_SOURCE_OTHER,
  SL_DEVICE_SOURCE_WLAN,
  SL_DEVICE_SOURCE_NETCFG,
  SL_DEVICE_SOURCE_NETAPP,
  SL_DEVICE_SOURCE_SECURITY,
  SL_DEVICE_SOURCE_LAST = 0xFF
}
 
enum  SlDeviceResetRequestCaller_e {
  SL_DEVICE_RESET_REQUEST_CALLER_PROVISIONING,
  SL_DEVICE_RESET_REQUEST_CALLER_PROVISIONING_EXTERNAL_CONFIGURATION,
  SL_DEVICE_RESET_REQUEST_NUM_OF_CALLERS
}
 

Detailed Description

Controls the behaviour of the CC31xx/CC32xx device (start/stop, events masking and obtaining specific device status)

Function Documentation

§ sl_DeviceEventMaskGet()

_i16 sl_DeviceEventMaskGet ( const _u8  EventClass,
_u32 *  pMask 
)

Get current event mask of the device.

Return the events bit mask from the device. In case event is masked, the device will not send that event.

Parameters
[in]EventClassThe classification groups that the mask is referred to. Need to be one of the following:
  • SL_DEVICE_EVENT_CLASS_GLOBAL
  • SL_DEVICE_EVENT_CLASS_DEVICE
  • SL_DEVICE_EVENT_CLASS_WLAN
  • SL_DEVICE_EVENT_CLASS_BSD
  • SL_DEVICE_EVENT_CLASS_NETAPP
  • SL_DEVICE_EVENT_CLASS_NETCFG
  • SL_DEVICE_EVENT_CLASS_FS
[out]pMaskPointer to mask bitmap where the value should be stored. Bitmasks are the same as in sl_DeviceEventMaskSet
Returns
Zero on success, or a negative value if an error occurred
See also
sl_DeviceEventMaskSet
Note
Belongs to ext_api
Warning
Example
  • Getting an event mask for WLAN class:
    _u32 maskWlan;
    sl_DeviceEventMaskGet(SL_DEVICE_EVENT_CLASS_WLAN,&maskWlan);

Definition at line 437 of file device.c.

438 {
439  _SlEventMaskGetMsg_u Msg;
440 
441  /* verify that this api is allowed. if not allowed then
442  ignore the API execution and return immediately with an error */
443  VERIFY_API_ALLOWED(SL_OPCODE_SILO_DEVICE);
444 
445  Msg.Cmd.Group = EventClass;
446 
447  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlEventMaskGetCmdCtrl, &Msg, NULL));
448 
449  *pMask = Msg.Rsp.Mask;
450 
451  return SL_RET_CODE_OK;
452 }

§ sl_DeviceEventMaskSet()

_i16 sl_DeviceEventMaskSet ( const _u8  EventClass,
const _u32  Mask 
)

Set asynchronous event mask.

Mask asynchronous events from the device.
Masked events do not generate asynchronous messages from the device.
By default - all events are active

Parameters
[in]EventClassThe classification groups that the mask is referred to. Need to be one of the following:
  • SL_DEVICE_EVENT_CLASS_DEVICE
  • SL_DEVICE_EVENT_CLASS_WLAN
  • SL_DEVICE_EVENT_CLASS_BSD
  • SL_DEVICE_EVENT_CLASS_NETAPP
  • SL_DEVICE_EVENT_CLASS_NETCFG
  • SL_DEVICE_EVENT_CLASS_FS
[in]MaskEvent Mask bitmap. Valid mask are (per group):
  • SL_DEVICE_EVENT_CLASS_WLAN user events
    • SL_WLAN_EVENT_CONNECT
    • SL_WLAN_EVENT_P2P_CONNECT
    • SL_WLAN_EVENT_DISCONNECT
    • SL_WLAN_EVENT_P2P_DISCONNECT
    • SL_WLAN_EVENT_STA_ADDED
    • SL_WLAN_EVENT_STA_REMOVED
    • SL_WLAN_EVENT_P2P_CLIENT_ADDED
    • SL_WLAN_EVENT_P2P_CLIENT_REMOVED
    • SL_WLAN_EVENT_P2P_DEVFOUND
    • SL_WLAN_EVENT_P2P_REQUEST
    • SL_WLAN_EVENT_P2P_CONNECTFAIL
    • SL_WLAN_EVENT_PROVISIONING_STATUS
    • SL_WLAN_EVENT_PROVISIONING_PROFILE_ADDED
    • SL_WLAN_EVENT_RXFILTER
  • SL_DEVICE_EVENT_CLASS_DEVICE user events
    • SL_DEVICE_EVENT_ERROR
  • SL_DEVICE_EVENT_CLASS_BSD user events
    • SL_SOCKET_TX_FAILED_EVENT
    • SL_SOCKET_ASYNC_EVENT
  • SL_DEVICE_EVENT_CLASS_NETAPP user events
    • SL_NETAPP_EVENT_IPV4_ACQUIRED
    • SL_NETAPP_EVENT_IPV6_ACQUIRED
    • SL_NETAPP_EVENT_DHCPV4_LEASED
    • SL_NETAPP_EVENT_DHCPV4_RELEASED
    • SL_NETAPP_EVENT_IP_COLLISION
    • SL_NETAPP_EVENT_IPV4_LOST
    • SL_NETAPP_EVENT_DHCP_IPV4_ACQUIRE_TIMEOUT
    • SL_NETAPP_EVENT_IPV6_LOST
Returns
Zero on success, or a negative value if an error occurred
Persistent System Persistent
See also
sl_DeviceEventMaskGet
Note
Belongs to ext_api
Warning
Example
  • Masking connection/disconnection async events from WLAN class:
    sl_DeviceEventMaskSet(SL_DEVICE_EVENT_CLASS_WLAN, (SL_DEVICE_EVENT_BIT(SL_WLAN_EVENT_CONNECT) | SL_DEVICE_EVENT_BIT(SL_WLAN_EVENT_DISCONNECT) ) );

Definition at line 399 of file device.c.

400 {
401  _SlEventMaskSetMsg_u Msg;
402 
403  /* verify that this api is allowed. if not allowed then
404  ignore the API execution and return immediately with an error */
405  VERIFY_API_ALLOWED(SL_OPCODE_SILO_DEVICE);
406 
407  Msg.Cmd.Group = EventClass;
408  Msg.Cmd.Mask = Mask;
409 
410  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlEventMaskSetCmdCtrl, &Msg, NULL));
411 
412  return (_i16)Msg.Rsp.status;
413 }

§ sl_DeviceGet()

_i16 sl_DeviceGet ( const _u8  DeviceGetId,
_u8 *  pOption,
_u16 *  pConfigLen,
_u8 *  pValues 
)

Internal function for getting device configurations.

Parameters
[in]DeviceGetIdconfiguration id:
  • SL_DEVICE_STATUS
  • SL_DEVICE_GENERAL
  • SL_DEVICE_IOT
[out]pOptionGet configurations option:
  • SL_DEVICE_STATUS:
    • SL_DEVICE_EVENT_CLASS_DEVICE
    • SL_DEVICE_EVENT_CLASS_WLAN
    • SL_DEVICE_EVENT_CLASS_BSD
    • SL_DEVICE_EVENT_CLASS_NETAPP
    • SL_DEVICE_EVENT_CLASS_NETCFG
    • SL_DEVICE_EVENT_CLASS_FS
  • SL_DEVICE_GENERAL:
    • SL_DEVICE_GENERAL_VERSION
    • SL_DEVICE_GENERAL_DATE_TIME
    • SL_DEVICE_GENERAL_PERSISTENT
  • SL_DEVICE_IOT:
    • SL_DEVICE_IOT_UDID
[out]pConfigLenThe length of the allocated memory as input, when the function complete, the value of this parameter would be the len that actually read from the device.
If the device return length that is longer from the input value, the function will cut the end of the returned structure and will return SL_ESMALLBUF
[out]pValuesGet requested configurations values
Returns
Zero on success, or a negative value if an error occurred
See also
Note
Warning
Examples
  • Getting WLAN class status (status is always cleared on read):
    _u32 statusWlan;
    _u8 pConfigOpt;
    _u16 pConfigLen;
    pConfigOpt = SL_DEVICE_EVENT_CLASS_WLAN;
    pConfigLen = sizeof(_u32);
    sl_DeviceGet(SL_DEVICE_STATUS,&pConfigOpt,&pConfigLen,(_u8 *)(&statusWlan));
    if (SL_DEVICE_STATUS_WLAN_STA_CONNECTED & statusWlan )
    {
    printf("Device is connected\n");
    }
    if (SL_DEVICE_EVENT_DROPPED_WLAN_RX_FILTERS & statusWlan )
    {
    printf("RX filer event dropped\n");
    }

  • Getting version:
    pConfigLen = sizeof(ver);
    pConfigOpt = SL_DEVICE_GENERAL_VERSION;
    sl_DeviceGet(SL_DEVICE_GENERAL,&pConfigOpt,&pConfigLen,(_u8 *)(&ver));
    printf("CHIP %d\nMAC 31.%d.%d.%d.%d\nPHY %d.%d.%d.%d\nNWP %d.%d.%d.%d\nROM %d\nHOST %d.%d.%d.%d\n",
    ver.ChipId,
    ver.FwVersion[0],ver.FwVersion[1],
    ver.FwVersion[2],ver.FwVersion[3],
    ver.PhyVersion[0],ver.PhyVersion[1],
    ver.PhyVersion[2],ver.PhyVersion[3],
    ver.NwpVersion[0],ver.NwpVersion[1],ver.NwpVersion[2],ver.NwpVersion[3],
    ver.RomVersion,
    SL_MAJOR_VERSION_NUM,SL_MINOR_VERSION_NUM,SL_VERSION_NUM,SL_SUB_VERSION_NUM);

  • Getting Device time and date:
    SlDateTime_t dateTime = {0};
    _i16 configLen = sizeof(SlDateTime_t);
    _i8 configOpt = SL_DEVICE_GENERAL_DATE_TIME;
    sl_DeviceGet(SL_DEVICE_GENERAL,&configOpt, &configLen,(_u8 *)(&dateTime));
    printf("Day %d,Mon %d,Year %d,Hour %,Min %d,Sec %d\n",dateTime.tm_day,dateTime.tm_mon,dateTime.tm_year,
    dateTime.tm_hour,dateTime.tm_min,dateTime.tm_sec);
  • Getting persistency system configuration:
    _i16 configLen = sizeof(_u8);
    _i8 configOpt = SL_DEVICE_GENERAL_PERSISTENT;
    sl_DeviceGet(SL_DEVICE_GENERAL,&configOpt, &configLen,&persistent);

Definition at line 478 of file device.c.

479 {
480  _SlDeviceMsgGet_u Msg;
481  _SlCmdExt_t CmdExt;
482 
483  /* verify that this api is allowed. if not allowed then
484  ignore the API execution and return immediately with an error */
485  VERIFY_API_ALLOWED(SL_OPCODE_SILO_DEVICE);
486 
487  if (*pConfigLen == 0)
488  {
489  return SL_EZEROLEN;
490  }
491 
492  if( pOption )
493  {
494 
495  _SlDrvResetCmdExt(&CmdExt);
496  CmdExt.RxPayloadLen = (_i16)*pConfigLen;
497  CmdExt.pRxPayload = (_u8 *)pValues;
498 
499  Msg.Cmd.DeviceSetId = DeviceGetId;
500 
501  Msg.Cmd.Option = (_u16)*pOption;
502 
503  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlDeviceGetCmdCtrl, &Msg, &CmdExt));
504 
505  if( pOption )
506  {
507  *pOption = (_u8)Msg.Rsp.Option;
508  }
509 
510  if (CmdExt.RxPayloadLen < CmdExt.ActualRxPayloadLen)
511  {
512  *pConfigLen = (_u16)CmdExt.RxPayloadLen;
513 
514  return SL_ESMALLBUF;
515  }
516  else
517  {
518  *pConfigLen = (_u16)CmdExt.ActualRxPayloadLen;
519  }
520 
521  return (_i16)Msg.Rsp.Status;
522  }
523  else
524  {
525  return SL_RET_CODE_INVALID_INPUT;
526  }
527 }

§ sl_DeviceSet()

_i16 sl_DeviceSet ( const _u8  DeviceSetId,
const _u8  Option,
const _u16  ConfigLen,
const _u8 *  pValues 
)

Setting device configurations.

Parameters
[in]DeviceSetIdconfiguration id:
  • SL_DEVICE_GENERAL
[in]Optionconfigurations option:
  • SL_DEVICE_GENERAL_DATE_TIME
  • SL_DEVICE_GENERAL_PERSISTENT
[in]ConfigLenconfigurations len
[in]pValuesconfigurations values
Returns
Zero on success, or a negative value if an error occurred
Persistent
SL_DEVICE_GENERAL_DATE_TIME - System Persistent (kept during hibernate only, See Note for details)
SL_DEVICE_GENERAL_PERSISTENT - Persistent
See also
Note
Persistency for SL_DEVICE_GENERAL_DATE_TIME - The original setted value will be kept as System Persistence.
The updated date and time though, will be kept during hibernate only.
Warning
Examples:
  • Setting device time and date example:
    SlDateTime_t dateTime= {0};
    dateTime.tm_day = (_u32)23; // Day of month (DD format) range 1-31
    dateTime.tm_mon = (_u32)6; // Month (MM format) in the range of 1-12
    dateTime.tm_year = (_u32)2014; // Year (YYYY format)
    dateTime.tm_hour = (_u32)17; // Hours in the range of 0-23
    dateTime.tm_min = (_u32)55; // Minutes in the range of 0-59
    dateTime.tm_sec = (_u32)22; // Seconds in the range of 0-59
    sl_DeviceSet(SL_DEVICE_GENERAL,
    SL_DEVICE_GENERAL_DATE_TIME,
    sizeof(SlDateTime_t),
    (_u8 *)(&dateTime));

  • Setting system persistent configuration:
    Sets the default system-wide configuration persistence mode. In case true, all APIs that follow 'system configured' persistence (see persistence attribute noted per API) shall maintain the configured settings. In case false, all calls to APIs that follow 'system configured' persistence shall be volatile. Configuration should revert to default after reset or power recycle
    _u8 persistent = 1;
    sl_DeviceSet(SL_DEVICE_GENERAL,
    SL_DEVICE_GENERAL_PERSISTENT,
    sizeof(_u8),
    (_u8 *)(&persistent));

Definition at line 550 of file device.c.

551 {
552  _SlDeviceMsgSet_u Msg;
553  _SlCmdExt_t CmdExt;
554 
555  /* verify that this api is allowed. if not allowed then
556  ignore the API execution and return immediately with an error */
557  VERIFY_API_ALLOWED(SL_OPCODE_SILO_DEVICE);
558 
559  _SlDrvResetCmdExt(&CmdExt);
560 
561  CmdExt.TxPayload1Len = (ConfigLen+3) & (~3);
562  CmdExt.pTxPayload1 = (_u8 *)pValues;
563 
564  Msg.Cmd.DeviceSetId = DeviceSetId;
565  Msg.Cmd.ConfigLen = ConfigLen;
566  Msg.Cmd.Option = Option;
567 
568  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlDeviceSetCmdCtrl, &Msg, &CmdExt));
569 
570  return (_i16)Msg.Rsp.status;
571 }

§ sl_DeviceUartSetMode()

_i16 sl_DeviceUartSetMode ( const SlDeviceUartIfParams_t pUartParams)

Setting the internal uart mode.

Parameters
[in]pUartParamsPointer to the uart configuration parameter set:
  • baudrate - up to 711 Kbps
  • flow control - enable/disable
  • comm port - the comm port number
Returns
On success zero is returned, otherwise - Failed.
Persistent Non- Persistent
See also
Note
Belongs to basic_api
Warning
This function must consider the host uart capability

Definition at line 721 of file device.c.

722 {
723  _SlUartSetModeMsg_u Msg;
724  _u32 magicCode = (_u32)0xFFFFFFFF;
725 
726  Msg.Cmd.BaudRate = pUartParams->BaudRate;
727  Msg.Cmd.FlowControlEnable = pUartParams->FlowControlEnable;
728 
729 
730  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlUartSetModeCmdCtrl, &Msg, NULL));
731 
732  /* cmd response OK, we can continue with the handshake */
733  if (SL_RET_CODE_OK == Msg.Rsp.status)
734  {
735  sl_IfMaskIntHdlr();
736 
737  /* Close the comm port */
738  sl_IfClose(g_pCB->FD);
739 
740  /* Re-open the comm port */
741  sl_IfOpen((void * )pUartParams, SL_IF_UART_REOPEN_FLAGS);
742 
743  sl_IfUnMaskIntHdlr();
744 
745  /* send the magic code and wait for the response */
746  sl_IfWrite(g_pCB->FD, (_u8* )&magicCode, 4);
747 
748  magicCode = UART_SET_MODE_MAGIC_CODE;
749  sl_IfWrite(g_pCB->FD, (_u8* )&magicCode, 4);
750 
751  /* clear magic code */
752  magicCode = 0;
753 
754  /* wait (blocking) till the magic code to be returned from device */
755  sl_IfRead(g_pCB->FD, (_u8* )&magicCode, 4);
756 
757  /* check for the received magic code matching */
758  if (UART_SET_MODE_MAGIC_CODE != magicCode)
759  {
760  _SL_ASSERT(0);
761  }
762  }
763 
764  return (_i16)Msg.Rsp.status;
765 }

§ sl_Start()

_i16 sl_Start ( const void *  pIfHdl,
_i8 *  pDevName,
const P_INIT_CALLBACK  pInitCallBack 
)

Start the SimpleLink device.

This function initialize the communication interface, set the enable pin of the device, and call to the init complete callback.

Parameters
[in]pIfHdlOpened Interface Object. In case the interface must be opened outside the SimpleLink Driver, the user might give the handler to be used in
any access of the communication interface with the device (UART/SPI).
The SimpleLink driver will open an interface port only if this parameter is null!
[in]pDevNameThe name of the device to open. Could be used when the pIfHdl is null, to transfer information to the open interface function
This pointer could be used to pass additional information to sl_IfOpen in case it is required (e.g. UART com port name)
[in]pInitCallBackPointer to function that would be called on completion of the initialization process.
If this parameter is NULL the function is blocked until the device initialization is completed, otherwise the function returns immediately.
Returns
Returns the current active role (STA/AP/P2P/TAG) or an error code:
  • ROLE_STA, ROLE_AP, ROLE_P2P, ROLE_TAG in case of success, otherwise in failure one of the following is return:
  • SL_ERROR_ROLE_STA_ERR (Failure to load MAC/PHY in STA role)
  • SL_ERROR_ROLE_AP_ERR (Failure to load MAC/PHY in AP role)
  • SL_ERROR_ROLE_P2P_ERR (Failure to load MAC/PHY in P2P role)
  • SL_ERROR_CALIB_FAIL (Failure of calibration)
  • SL_ERROR_FS_CORRUPTED_ERR (FS is corrupted, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram))
  • SL_ERROR_FS_ALERT_ERR (Device is locked, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram))
  • SL_ERROR_RESTORE_IMAGE_COMPLETE (Return to factory image completed, perform reset)
  • SL_ERROR_ROLE_TAG_ERR (Failure to start TAG role)
  • SL_ERROR_FIPS_ERR (Failure to start with FIPS mode enabled)
  • SL_ERROR_GENERAL_ERR (General error during init)
See also
sl_Stop
Note
Belongs to basic_api
Warning
This function must be called before any other SimpleLink API is used, or after sl_Stop is called for reinit the device
Example:
  • Open interface without callback routine. The interface name and handler are handled by the sl_IfOpen routine:
    if( sl_Start(NULL, NULL, NULL) < 0 )
    {
    LOG("Error opening interface to device\n");
    }

  • Open interface with a callback routine:
    void SimpleLinkInitCallback(_u32 status)
    {
    LOG("Handle SimpleLink Interface acording to ststus %d\n", status);
    }
    void main(void)
    {
    if (sl_Start(NULL, NULL, SimpleLinkInitCallback) < 0)
    {
    LOG("Error opening interface to device\n");
    }
    }

Definition at line 119 of file device.c.

120 {
121  _u8 ObjIdx = MAX_CONCURRENT_ACTIONS;
122  InitComplete_t AsyncRsp;
123 
124  _SlDrvMemZero(&AsyncRsp, sizeof(InitComplete_t));
125 
126  /* verify no error handling in progress. if in progress than
127  ignore the API execution and return immediately with an error */
128  VERIFY_NO_ERROR_HANDLING_IN_PROGRESS();
129  if (SL_IS_DEVICE_STARTED)
130  {
131  return SL_RET_CODE_DEV_ALREADY_STARTED;
132  }
133  /* Perform any preprocessing before enable networking services */
134 #ifdef sl_DeviceEnablePreamble
135  sl_DeviceEnablePreamble();
136 #endif
137 
138  /* ControlBlock init */
139  (void)_SlDrvDriverCBInit();
140 
141  /* open the interface: usually SPI or UART */
142  if (NULL == pIfHdl)
143  {
144  g_pCB->FD = sl_IfOpen((void *)pDevName, SL_IF_OPEN_FLAGS);
145  }
146  else
147  {
148  g_pCB->FD = (_SlFd_t)pIfHdl;
149  }
150 
151  ObjIdx = _SlDrvProtectAsyncRespSetting((_u8 *)&AsyncRsp, START_STOP_ID, SL_MAX_SOCKETS);
152 
153  if (MAX_CONCURRENT_ACTIONS == ObjIdx)
154  {
155  return SL_POOL_IS_EMPTY;
156  }
157 
158  if( g_pCB->FD >= (_SlFd_t)0)
159  {
160  /* store the interface parameters for the internal call of the
161  sl_start to be called upon reset request handling */
162  DeviceCB.pIfHdl = pIfHdl;
163  DeviceCB.pDevName = pDevName;
164 
165  /* Mark that device is in progress! */
166  SL_SET_DEVICE_START_IN_PROGRESS;
167 
168  sl_DeviceDisable();
169 
170  sl_IfRegIntHdlr((SL_P_EVENT_HANDLER)_SlDrvRxIrqHandler, NULL);
171 
172  g_pCB->pInitCallback = pInitCallBack;
173  sl_DeviceEnable();
174 
175  if (NULL == pInitCallBack)
176  {
177 
178  VERIFY_RET_OK(_SlDrvWaitForInternalAsyncEvent(ObjIdx, INIT_COMPLETE_TIMEOUT, SL_OPCODE_DEVICE_INITCOMPLETE));
179 
180  SL_UNSET_DEVICE_START_IN_PROGRESS;
181 
182  SL_SET_DEVICE_STARTED;
183 
184  /* release Pool Object */
185  _SlDrvReleasePoolObj(g_pCB->FunctionParams.AsyncExt.ActionIndex);
186  return _SlDeviceGetStartResponseConvert(AsyncRsp.Status);
187  }
188  else
189  {
190  return SL_RET_CODE_OK;
191  }
192  }
193  return SL_BAD_INTERFACE;
194 }

§ sl_Stop()

_i16 sl_Stop ( const _u16  Timeout)

Stop the SimpleLink device.

This function clears the enable pin of the device, closes the communication
interface and invokes the stop complete callback

Parameters
[in]TimeoutStop timeout in msec. Should be used to give the device time to finish
any transmission/reception that is not completed when the function was called.
Additional options:
  • 0 Enter to hibernate immediately
  • 0xFFFF Host waits for device's response before
    hibernating, without timeout protection
  • 0 < Timeout[msec] < 0xFFFF Host waits for device's response before
    hibernating, with a defined timeout protection
    This timeout defines the max time to wait. The NWP
    response can be sent earlier than this timeout.
Returns
Zero on success, or a negative value if an error occurred
See also
sl_Start
Note
This API will shutdown the device and invoke the "i/f close" function regardless
if it was opened implicitly or explicitly.
It is up to the platform interface library to properly handle interface close
routine
Belongs to basic_api
Warning

Definition at line 273 of file device.c.

274 {
275  _i16 RetVal=0;
276  _SlStopMsg_u Msg;
277  _BasicResponse_t AsyncRsp;
278  _u8 ObjIdx = MAX_CONCURRENT_ACTIONS;
279  _u8 ReleasePoolObject = FALSE;
280  _u8 IsProvInProgress = FALSE;
281 
282  /* NOTE: don't check VERIFY_API_ALLOWED(), this command is not
283  * filtered in error handling and also not filtered in NWP lock state.
284  * If we are in the middle of assert handling than ignore stopping
285  * the device with timeout and force immediate shutdown as we would like
286  * to avoid any additional commands to the NWP */
287  if( (Timeout != 0) && (SL_IS_DEVICE_STARTED)
288  && (!SL_IS_RESTART_REQUIRED))
289  {
290  /* Clear the Async response structure */
291  _SlDrvMemZero(&AsyncRsp, sizeof(_BasicResponse_t));
292 
293  /* let the device make the shutdown using the defined timeout */
294  Msg.Cmd.Timeout = Timeout;
295 
296  IsProvInProgress = SL_IS_PROVISIONING_IN_PROGRESS;
297 
298  /* if provisioning in progress do not take pool object as we are not going to wait for it */
299  if (!IsProvInProgress)
300  {
301  ObjIdx = _SlDrvProtectAsyncRespSetting((_u8 *)&AsyncRsp, START_STOP_ID, SL_MAX_SOCKETS);
302  if (MAX_CONCURRENT_ACTIONS == ObjIdx)
303  {
304  return SL_POOL_IS_EMPTY;
305  }
306 
307  ReleasePoolObject = TRUE;
308  }
309 
310  /* Set the stop-in-progress flag */
311  SL_SET_DEVICE_STOP_IN_PROGRESS;
312 
313  VERIFY_RET_OK(_SlDrvCmdOp((_SlCmdCtrl_t *)&_SlStopCmdCtrl, &Msg, NULL));
314 
315  /* Do not wait for stop async event if provisioning is in progress */
316  if((SL_OS_RET_CODE_OK == (_i16)Msg.Rsp.status) && (!(IsProvInProgress)))
317  {
318  /* Wait for sync object to be signaled */
319  VERIFY_RET_OK(_SlDrvWaitForInternalAsyncEvent(ObjIdx, STOP_DEVICE_TIMEOUT, SL_OPCODE_DEVICE_STOP_ASYNC_RESPONSE));
320  Msg.Rsp.status = AsyncRsp.status;
321  RetVal = Msg.Rsp.status;
322  }
323 
324  /* Release pool object only if taken */
325  if (ReleasePoolObject == TRUE)
326  {
327  _SlDrvReleasePoolObj(ObjIdx);
328  }
329 
330  /* This macro wait for the NWP to raise a ready for shutdown indication.
331  * This function is unique for the CC32XX family, and expected to return
332  * in less than 600 mSec, which is the time takes for NWP to gracefully shutdown. */
333  WAIT_NWP_SHUTDOWN_READY;
334  }
335  else
336  {
337  if ((!SL_IS_DEVICE_STARTED)
338  && (!SL_IS_RESTART_REQUIRED))
339  {
340  sl_DeviceDisable();
341  return SL_RET_CODE_DEV_NOT_STARTED;
342  }
343  /* Set the stop-in-progress flag */
344  SL_SET_DEVICE_STOP_IN_PROGRESS;
345  }
346  /* Release (signal) all active and pending commands */
347  _SlDrvReleaseAllActivePendingPoolObj();
348 
349 #ifdef SL_PLATFORM_MULTI_THREADED
350  /* Do not continue until all sync object deleted (in relevant context) */
351  while (g_pCB->NumOfDeletedSyncObj < MAX_CONCURRENT_ACTIONS)
352  {
353  usleep(100000);
354  }
355 #endif
356 
357  /* Lock during stopping the interface */
358  SL_DRV_LOCK_GLOBAL_LOCK_FOREVER(GLOBAL_LOCK_FLAGS_NONE);
359 
360  sl_IfRegIntHdlr(NULL, NULL);
361  sl_DeviceDisable();
362  RetVal = sl_IfClose(g_pCB->FD);
363 
364  (void)_SlDrvDriverCBDeinit();
365 
366  /* clear the stop-in-progress flag */
367  SL_UNSET_DEVICE_STOP_IN_PROGRESS;
368 
369  /* clear the device started flag */
370  SL_UNSET_DEVICE_STARTED;
371 
372  SL_DRV_LOCK_GLOBAL_UNLOCK(FALSE);
373 
374  return RetVal;
375 }

§ sl_Task()

void* sl_Task ( void *  pEntry)

The SimpleLink task entry.

This function must be called from the main loop or from dedicated thread in the following cases:

  • Non-Os Platform - should be called from the mail loop
  • Multi Threaded Platform when the user does not implement the external spawn functions - should be called from dedicated thread allocated to the SimpleLink driver. In this mode the function never return.
parameters
None
Returns
None
See also
Note
Belongs to basic_api
Warning
This function must be called from a thread that is start running before any call to other SimpleLink API

Definition at line 105 of file device.c.

106 {
107 #ifdef _SlTaskEntry
108  return (void*)_SlTaskEntry();
109 #else
110  return (void*)0;
111 #endif
112 }

§ sl_WifiConfig()

_i32 sl_WifiConfig ( )

Configure SimpleLink to default state.

The sl_WifiConfig function allows to configure the device to a pre-configured state by sysconfig UI\ ti_drivers_net_wifi_Config.c. The configuration of the SimpleLink Wifi is usually persistent, and can be reconfigured at runtime. Reconfiguration should be performed only when needed since the process involves flash writes and might impact system lifetime (flash write endurance) and power consumption.

It's important to note that this is one example for a 'restore to default state' function, which meet the needs of this application. User who wish to incorporate this function into he's app, must adjust the implementation and make sure it meets he's needs.

Returns
Upon successful completion, the function shall return 0. In case of failure, this function would return -1.

Definition at line 46 of file wlanconfig.c.

47 {
48  _u8 ucConfigOpt;
49  _u16 uIPMode;
50  _i32 RetVal = -1;
51  _i32 RetVal_stop = -1;
52  _i32 Mode = -1;
53  SlNetCfgIpV4Args_t *ipV4 = NULL;
54  SlNetCfgIpV4Args_t localIpV4;
55  _u16 ipConfigSize = 0;
56 
57 
58  /* Turn NWP on */
59  Mode = sl_Start(NULL, NULL, NULL);
60  if (Mode < 0)
61  {
62  return Mode;
63  }
64 
65  while (1)
66  {
67  if ((SimpleLinkWifiCC32XX_config.Mode != SL_DEVICE_SYSCONFIG_AS_CONFIGURED) && (SimpleLinkWifiCC32XX_config.Mode != Mode))
68  {
69  /* Set NWP role */
70  RetVal = sl_WlanSetMode(SimpleLinkWifiCC32XX_config.Mode);
71  if (RetVal < 0)
72  {
73  break;
74  }
75 
76  /* For changes to take affect, we restart the NWP */
77  RetVal = sl_Stop(200);
78  if (RetVal < 0)
79  {
80  break;
81  }
82 
83  RetVal = sl_Start(NULL, NULL, NULL);
84  if (RetVal < 0)
85  {
86  break;
87  }
88 
89  if(SimpleLinkWifiCC32XX_config.Mode != RetVal)
90  {
91  RetVal = -1;
92  break;
93  }
94  }
95 
96  /* Set connection policy */
97  if (SimpleLinkWifiCC32XX_config.ConnectionPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
98  {
99  RetVal =
100  sl_WlanPolicySet(SL_WLAN_POLICY_CONNECTION,
101  SimpleLinkWifiCC32XX_config.ConnectionPolicy,
102  NULL,0);
103  if (RetVal < 0)
104  {
105  break;
106  }
107  }
108  if (SimpleLinkWifiCC32XX_config.ProvisioningStop)
109  {
110  /* Stop Provisioning */
111  RetVal = sl_WlanProvisioning(SL_WLAN_PROVISIONING_CMD_STOP,
112  0xFF,
113  0,
114  NULL,
115  0x0);
116  if (RetVal < 0)
117  {
118  break;
119  }
120  }
121  if (SimpleLinkWifiCC32XX_config.DeleteAllProfile)
122  {
123  /* Delete existing profiles */
124  RetVal = sl_WlanProfileDel(SL_WLAN_DEL_ALL_PROFILES);
125  if (RetVal < 0)
126  {
127  break;
128  }
129  }
130 
131  /* Configure ipv4/DHCP */
132  if (SimpleLinkWifiCC32XX_config.Ipv4Config != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
133  {
134  if (SimpleLinkWifiCC32XX_config.Mode == ROLE_STA)
135  {
136  uIPMode = SL_NETCFG_IPV4_STA_ADDR_MODE;
137  }
138  else if (SimpleLinkWifiCC32XX_config.Mode == ROLE_AP)
139  {
140  uIPMode = SL_NETCFG_IPV4_AP_ADDR_MODE;
141  }
142  if (SimpleLinkWifiCC32XX_config.Ipv4Config == SL_NETCFG_ADDR_STATIC)
143  {
144  ipV4 = &localIpV4;
145  ipConfigSize = sizeof(SlNetCfgIpV4Args_t);
146 
147  localIpV4.Ip = (_u32)SimpleLinkWifiCC32XX_config.Ipv4; // _u32 IP address
148  localIpV4.IpMask = (_u32)SimpleLinkWifiCC32XX_config.IpMask; // _u32 Subnet mask for this AP/P2P
149  localIpV4.IpGateway = (_u32)SimpleLinkWifiCC32XX_config.IpGateway; // _u32 Default gateway address
150  localIpV4.IpDnsServer = (_u32)SimpleLinkWifiCC32XX_config.IpDnsServer; // _u32 DNS server address
151  }
152  else if (SimpleLinkWifiCC32XX_config.Ipv4Config != SL_NETCFG_ADDR_DHCP)
153  {
154  RetVal = -1;
155  if (RetVal < 0)
156  {
157  break;
158  }
159  }
160 
161  RetVal = sl_NetCfgSet(uIPMode, SimpleLinkWifiCC32XX_config.Ipv4Config, ipConfigSize, (_u8 *)ipV4);
162  if (RetVal < 0)
163  {
164  break;
165  }
166  }
167 
168  /* Set scan policy */
169  if (SimpleLinkWifiCC32XX_config.ScanPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
170  {
171  _u32 intervalInSeconds = SimpleLinkWifiCC32XX_config.ScanIntervalInSeconds;
172  ucConfigOpt = SimpleLinkWifiCC32XX_config.ScanPolicy;
173  RetVal = sl_WlanPolicySet(SL_WLAN_POLICY_SCAN, ucConfigOpt, (_u8 *)&intervalInSeconds, sizeof(intervalInSeconds));
174  if (RetVal < 0)
175  {
176  break;
177  }
178  }
179 
180  /* Set NWP Power Management Policy */
181  if (SimpleLinkWifiCC32XX_config.PMPolicy != SL_DEVICE_SYSCONFIG_AS_CONFIGURED)
182  {
183  if (SimpleLinkWifiCC32XX_config.PMPolicy != SL_WLAN_LONG_SLEEP_INTERVAL_POLICY)
184  {
185  RetVal = sl_WlanPolicySet(SL_WLAN_POLICY_PM, SimpleLinkWifiCC32XX_config.PMPolicy, NULL,0);
186  if (RetVal < 0)
187  {
188  break;
189  }
190  }
191  else
192  {
193  SlWlanPmPolicyParams_t PmPolicyParams;
194  memset(&PmPolicyParams,0,sizeof(SlWlanPmPolicyParams_t));
195  PmPolicyParams.MaxSleepTimeMs = SimpleLinkWifiCC32XX_config.MaxSleepTimeMS; //max sleep time in mSec
196  RetVal = sl_WlanPolicySet(SL_WLAN_POLICY_PM, SimpleLinkWifiCC32XX_config.PMPolicy, (_u8*)&PmPolicyParams, sizeof(PmPolicyParams));
197  if (RetVal < 0)
198  {
199  break;
200  }
201  }
202  }
203 
204  /* Set DHCP Server Configuration */
205  if (SimpleLinkWifiCC32XX_config.DHCPServer)
206  {
207  SlNetAppDhcpServerBasicOpt_t dhcpParams;
208  _u8 outLen = sizeof(SlNetAppDhcpServerBasicOpt_t);
209  dhcpParams.lease_time = SimpleLinkWifiCC32XX_config.LeaseTime; // lease time (in seconds) of the IP Address
210  dhcpParams.ipv4_addr_start = (_u32)SimpleLinkWifiCC32XX_config.StartAddress; // first IP Address for allocation. IP Address should be set as Hex number - i.e. 0A0B0C01 for (10.11.12.1)
211  dhcpParams.ipv4_addr_last = (_u32)SimpleLinkWifiCC32XX_config.LastAddress; // last IP Address for allocation. IP Address should be set as Hex number - i.e. 0A0B0C01 for (10.11.12.1)
212  RetVal = sl_NetAppStop(SL_NETAPP_DHCP_SERVER_ID); // Stop DHCP server before settings
213  if (RetVal < 0)
214  {
215  break;
216  }
217  RetVal = sl_NetAppSet(SL_NETAPP_DHCP_SERVER_ID, SL_NETAPP_DHCP_SRV_BASIC_OPT, outLen, (_u8* )&dhcpParams); // set parameters
218  if (RetVal < 0)
219  {
220  break;
221  }
222  if (SimpleLinkWifiCC32XX_config.Mode == ROLE_AP)
223  {
224  RetVal = sl_NetAppStart(SL_NETAPP_DHCP_SERVER_ID); // Start DHCP server with new settings
225  if (RetVal < 0)
226  {
227  break;
228  }
229  }
230  }
231  else
232  {
233  sl_NetAppStop(SL_NETAPP_HTTP_SERVER_ID);
234  }
235  break;
236  }
237  /* Jump here if error occurred or after all the configurations was set successfully */
238  /* For changes to take affect, we restart the NWP - sl_start will be call by application */
239  RetVal_stop = sl_Stop(200);
240  if (RetVal_stop < 0)
241  {
242  return RetVal_stop;
243  }
244  return(RetVal);
245 }
_i16 sl_WlanSetMode(const _u8 Mode)
Wlan set mode.
Definition: wlan.c:1090
_i16 sl_NetAppSet(const _u8 AppId, const _u8 Option, const _u8 OptionLen, const _u8 *pOptionValue)
Setting network application configurations.
Definition: netapp.c:1110
_i16 sl_WlanProvisioning(_u8 ProvisioningCmd, _u8 RequestedRoleAfterSuccess, _u16 InactivityTimeoutSec, char *pSmartConfigKey, _u32 Flags)
The simpleLink will switch to the appropriate role according to the provisioning mode requested and w...
Definition: wlan.c:1026
_i16 sl_Stop(const _u16 Timeout)
Stop the SimpleLink device.
Definition: device.c:273
_i16 sl_WlanPolicySet(const _u8 Type, const _u8 Policy, _u8 *pVal, const _u8 ValLen)
Set policy values.
Definition: wlan.c:242
_i16 sl_NetCfgSet(const _u16 ConfigId, const _u16 ConfigOpt, const _u16 ConfigLen, const _u8 *pValues)
Setting network configurations.
Definition: netcfg.c:63
_i16 sl_WlanProfileDel(const _i16 Index)
Delete WLAN profile.
Definition: wlan.c:786
_i16 sl_NetAppStart(const _u32 AppBitMap)
Starts a network application.
Definition: netapp.c:103
_i16 sl_NetAppStop(const _u32 AppBitMap)
Stops a network application.
Definition: netapp.c:129
_i16 sl_Start(const void *pIfHdl, _i8 *pDevName, const P_INIT_CALLBACK pInitCallBack)
Start the SimpleLink device.
Definition: device.c:119

Data Structure Documentation

§ SlDeviceEventResetRequest_t

struct SlDeviceEventResetRequest_t

Definition at line 87 of file device.h.

Data Fields
_u16 Caller
_i16 Status

§ SlDeviceEventError_t

struct SlDeviceEventError_t

Definition at line 104 of file device.h.

Data Fields
_i16 Code
SlDeviceSource_e Source

§ SlDeviceEventData_u

union SlDeviceEventData_u

Definition at line 110 of file device.h.

Data Fields
SlDeviceEventError_t Error
SlDeviceEventResetRequest_t ResetRequest

§ SlDeviceEvent_t

struct SlDeviceEvent_t

Definition at line 125 of file device.h.

Data Fields
SlDeviceEventData_u Data
_u32 Id

§ SlDeviceFatalDeviceAssert_t

struct SlDeviceFatalDeviceAssert_t

Definition at line 139 of file device.h.

Data Fields
_u32 Code
_u32 Value

§ SlDeviceFatalNoCmdAck_t

struct SlDeviceFatalNoCmdAck_t

Definition at line 146 of file device.h.

Data Fields
_u32 Code

§ SlDeviceFatalData_u

union SlDeviceFatalData_u

Definition at line 152 of file device.h.

Data Fields
SlDeviceFatalCmdTimeout_t CmdTimeout
SlDeviceFatalDeviceAssert_t DeviceAssert
SlDeviceFatalNoCmdAck_t NoCmdAck

§ SlDeviceFatal_t

struct SlDeviceFatal_t

Definition at line 160 of file device.h.

Data Fields
SlDeviceFatalData_u Data
_u32 Id

§ SlDeviceUartIfParams_t

struct SlDeviceUartIfParams_t

Definition at line 235 of file device.h.

Data Fields
_u32 BaudRate
_u8 CommPort
_u8 FlowControlEnable

§ SlDeviceVersion_t

struct SlDeviceVersion_t

Definition at line 257 of file device.h.

Data Fields
_u32 ChipId
_u8 FwVersion[4]
_u8 NwpVersion[4]
_u16 Padding
_u8 PhyVersion[4]
_u16 RomVersion

§ SlDateTime_t

struct SlDateTime_t

Definition at line 268 of file device.h.

Data Fields
_u32 reserved[3]
_u32 tm_day
_u32 tm_hour
_u32 tm_min
_u32 tm_mon
_u32 tm_sec
_u32 tm_week_day
_u32 tm_year
_u32 tm_year_day

§ SlDeviceInitInfo_t

struct SlDeviceInitInfo_t

Definition at line 289 of file device.h.

Data Fields
_u32 ChipId
_u32 MoreData