![]() |
![]() |
UARTCC32XXDMA Object. More...
#include <UARTCC32XXDMA.h>

Data Fields | |
| bool | opened |
| UART_Mode | readMode |
| UART_Mode | writeMode |
| unsigned int | readTimeout |
| unsigned int | writeTimeout |
| UART_Callback | readCallback |
| UART_Callback | writeCallback |
| UART_ReturnMode | readReturnMode |
| UART_DataMode | readDataMode |
| UART_DataMode | writeDataMode |
| uint32_t | baudRate |
| UART_LEN | dataLength |
| UART_STOP | stopBits |
| UART_PAR | parityType |
| UART_Echo | readEcho |
| const void * | writeBuf |
| size_t | writeCount |
| size_t | writeSize |
| void * | readBuf |
| size_t | readCount |
| size_t | readSize |
| SemaphoreP_Handle | writeSem |
| SemaphoreP_Handle | readSem |
| HwiP_Handle | hwiHandle |
| ClockP_Handle | txFifoEmptyClk |
| Power_NotifyObj | postNotify |
| unsigned int | powerMgrId |
| PowerCC32XX_ParkState | prevParkTX |
| uint16_t | txPin |
| PowerCC32XX_ParkState | prevParkRTS |
| uint16_t | rtsPin |
| UDMACC32XX_Handle | dmaHandle |
UARTCC32XXDMA Object.
The application must not access any member variables of this structure!
| bool UARTCC32XXDMA_Object::opened |
| UART_Mode UARTCC32XXDMA_Object::readMode |
| UART_Mode UARTCC32XXDMA_Object::writeMode |
| unsigned int UARTCC32XXDMA_Object::readTimeout |
| unsigned int UARTCC32XXDMA_Object::writeTimeout |
| UART_Callback UARTCC32XXDMA_Object::readCallback |
| UART_Callback UARTCC32XXDMA_Object::writeCallback |
| UART_ReturnMode UARTCC32XXDMA_Object::readReturnMode |
| UART_DataMode UARTCC32XXDMA_Object::readDataMode |
| UART_DataMode UARTCC32XXDMA_Object::writeDataMode |
| uint32_t UARTCC32XXDMA_Object::baudRate |
| UART_LEN UARTCC32XXDMA_Object::dataLength |
| UART_STOP UARTCC32XXDMA_Object::stopBits |
| UART_PAR UARTCC32XXDMA_Object::parityType |
| UART_Echo UARTCC32XXDMA_Object::readEcho |
| const void* UARTCC32XXDMA_Object::writeBuf |
| size_t UARTCC32XXDMA_Object::writeCount |
| size_t UARTCC32XXDMA_Object::writeSize |
| void* UARTCC32XXDMA_Object::readBuf |
| size_t UARTCC32XXDMA_Object::readCount |
| size_t UARTCC32XXDMA_Object::readSize |
| SemaphoreP_Handle UARTCC32XXDMA_Object::writeSem |
| SemaphoreP_Handle UARTCC32XXDMA_Object::readSem |
| HwiP_Handle UARTCC32XXDMA_Object::hwiHandle |
| ClockP_Handle UARTCC32XXDMA_Object::txFifoEmptyClk |
| Power_NotifyObj UARTCC32XXDMA_Object::postNotify |
| unsigned int UARTCC32XXDMA_Object::powerMgrId |
| PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkTX |
| uint16_t UARTCC32XXDMA_Object::txPin |
| PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkRTS |
| uint16_t UARTCC32XXDMA_Object::rtsPin |
| UDMACC32XX_Handle UARTCC32XXDMA_Object::dmaHandle |