Data Fields
SPICC32XXDMA_Object Struct Reference

SPICC32XXDMA Object. More...

#include <SPICC32XXDMA.h>

Collaboration diagram for SPICC32XXDMA_Object:
Collaboration graph
[legend]

Data Fields

HwiP_Handle hwiHandle
 
Power_NotifyObj notifyObj
 
SemaphoreP_Handle transferComplete
 
SPI_CallbackFxn transferCallbackFxn
 
SPI_Transactiontransaction
 
UDMACC32XX_Handle dmaHandle
 
size_t amtDataXferred
 
size_t currentXferAmt
 
uint32_t bitRate
 
uint32_t dataSize
 
uint32_t transferTimeout
 
SPI_Mode spiMode
 
SPI_TransferMode transferMode
 
SPI_FrameFormat frameFormat
 
bool cancelInProgress
 
bool isOpen
 
uint8_t rxFifoTrigger
 
uint8_t txFifoTrigger
 

Detailed Description

SPICC32XXDMA Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle SPICC32XXDMA_Object::hwiHandle

§ notifyObj

Power_NotifyObj SPICC32XXDMA_Object::notifyObj

§ transferComplete

SemaphoreP_Handle SPICC32XXDMA_Object::transferComplete

§ transferCallbackFxn

SPI_CallbackFxn SPICC32XXDMA_Object::transferCallbackFxn

§ transaction

SPI_Transaction* SPICC32XXDMA_Object::transaction

§ dmaHandle

UDMACC32XX_Handle SPICC32XXDMA_Object::dmaHandle

§ amtDataXferred

size_t SPICC32XXDMA_Object::amtDataXferred

§ currentXferAmt

size_t SPICC32XXDMA_Object::currentXferAmt

§ bitRate

uint32_t SPICC32XXDMA_Object::bitRate

§ dataSize

uint32_t SPICC32XXDMA_Object::dataSize

§ transferTimeout

uint32_t SPICC32XXDMA_Object::transferTimeout

§ spiMode

SPI_Mode SPICC32XXDMA_Object::spiMode

§ transferMode

SPI_TransferMode SPICC32XXDMA_Object::transferMode

§ frameFormat

SPI_FrameFormat SPICC32XXDMA_Object::frameFormat

§ cancelInProgress

bool SPICC32XXDMA_Object::cancelInProgress

§ isOpen

bool SPICC32XXDMA_Object::isOpen

§ rxFifoTrigger

uint8_t SPICC32XXDMA_Object::rxFifoTrigger

§ txFifoTrigger

uint8_t SPICC32XXDMA_Object::txFifoTrigger

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale