Macros
Collaboration diagram for Command Codes:

Macros

#define WatchdogCC32XX_CMD_IS_TIMER_ENABLE   (Watchdog_CMD_RESERVED + 0)
 Command used by Watchdog_control to determines whether the watchdog timer is enabled. More...
 
#define WatchdogCC32XX_CMD_GET_TIMER_VALUE   (Watchdog_CMD_RESERVED + 1)
 Command used by Watchdog_control to gets the current watchdog timer value. More...
 
#define WatchdogCC32XX_CMD_IS_TIMER_LOCKED   (Watchdog_CMD_RESERVED + 2)
 Command used by Watchdog_control to determines whether the watchdog timer is locked. More...
 
#define WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE   (Watchdog_CMD_RESERVED + 3)
 Command used by Watchdog_control to gets the current watchdog timer reload value. More...
 

Detailed Description

Watchdog_CMD_* macros are general command codes for Watchdog_control(). Not all Watchdog driver implementations support these command codes.

WatchdogCC32XX_CMD_* macros are command codes only defined in the WatchdogCC32XX.h driver implementation and need to:

Macro Definition Documentation

§ WatchdogCC32XX_CMD_IS_TIMER_ENABLE

#define WatchdogCC32XX_CMD_IS_TIMER_ENABLE   (Watchdog_CMD_RESERVED + 0)

Command used by Watchdog_control to determines whether the watchdog timer is enabled.

With this command code, arg is a pointer to a bool. *arg contains true if the watchdog timer is enabled, else false if it is not.

§ WatchdogCC32XX_CMD_GET_TIMER_VALUE

#define WatchdogCC32XX_CMD_GET_TIMER_VALUE   (Watchdog_CMD_RESERVED + 1)

Command used by Watchdog_control to gets the current watchdog timer value.

With this command code, arg is a pointer to an integer. *arg contains the current value of the watchdog timer.

§ WatchdogCC32XX_CMD_IS_TIMER_LOCKED

#define WatchdogCC32XX_CMD_IS_TIMER_LOCKED   (Watchdog_CMD_RESERVED + 2)

Command used by Watchdog_control to determines whether the watchdog timer is locked.

With this command code, arg is a pointer to a bool. *arg contains true if the watchdog timer is locked, else false if it is not.

§ WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE

#define WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE   (Watchdog_CMD_RESERVED + 3)

Command used by Watchdog_control to gets the current watchdog timer reload value.

With this command code, arg is a pointer to an integer. *arg contains the current value loaded into the watchdog timer when the count reaches zero for the first time.

© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale