![]() |
![]() |
Capture driver interface.
The capture header file should be included in an application as follows:
The capture driver serves as the main interface for a typical RTOS application. Its purpose is to redirect the capture APIs to device specific implementations which are specified using a pointer to a Capture_FxnTable. The device specific implementations are responsible for creating all the RTOS specific primitives to allow for thead-safe operation. The capture driver utilizes the general purpose timer hardware.
The capture driver internally handles the general purpose timer resource allocation. For each capture driver instance, Capture_open() occupies the specified timer, and Capture_close() releases the occupied timer resource.
The capture driver is used to detect and time edge triggered events on a GPIO pin. The following example code opens a capture instance in falling edge mode. The interval returned in the callback function is in microseconds.
In order to use the capture APIs, the application is required to provide device specific capture configuration in the Board.c file. The capture driver interface defines a configuration data structure:
The application must declare an array of Capture_Config elements, named Capture_config[]. Each element of Capture_config[] is populated with pointers to a device specific capture driver implementation's function table, driver object, and hardware attributes. The hardware attributes define properties such as the timer peripheral's base address, interrupt number and interrupt priority. Each element in Capture_config[] corresponds to a capture instance, and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation.
You will need to check the device specific capture driver implementation's header file for example configuration.
Capture_init() must be called before any other capture APIs. This function calls the device implementation's capture initialization function, for each element of Capture_config[].
The capture driver supports four modes of operation which may be specified in the Capture_Params.
Capture_RISING_EDGE will capture rising edge triggers. After Capture_start() is called, the callback function specified in Capture_Params will be called after each rising edge is detected on the GPIO pin. This behavior will continue until Capture_stop() is called.
Capture_FALLING_EDGE will capture falling edge triggers. After Capture_start() is called, the callback function specified in Capture_Params will be called after each falling edge is detected on the GPIO pin. This behavior will continue until Capture_stop() is called.
Capture_ANY_EDGE will capture both rising and falling edge triggers. After Capture_start() is called, the callback function specified in Capture_Params will be called after each rising or falling edge is detected on the GPIO pin. This behavior will continue until Capture_stop() is called.
The capture driver interface module is joined (at link time) to an array of Capture_Config data structures named Capture_config. Capture_config is implemented in the application with each entry being an instance of a capture peripheral. Each entry in Capture_config contains a:
The capture APIs are redirected to the device specific implementations using the Capture_FxnTable pointer of the Capture_config entry. In order to use device specific functions of the capture driver directly, link in the correct driver library for your device and include the device specific capture driver header file (which in turn includes Capture.h). For example, for the MSP432 family of devices, you would include the following header file:
#include <stdint.h>

Go to the source code of this file.
Data Structures | |
| struct | Capture_Params_ |
| Capture Parameters. More... | |
| struct | Capture_FxnTable_ |
| The definition of a capture function table that contains the required set of functions to control a specific capture driver implementation. More... | |
| struct | Capture_Config_ |
| Capture Global configuration. More... | |
Macros | |
| #define | Capture_CMD_RESERVED (32) |
| #define | Capture_STATUS_RESERVED (-32) |
| #define | Capture_STATUS_SUCCESS (0) |
| Successful status code. More... | |
| #define | Capture_STATUS_ERROR (-1) |
| Generic error status code. More... | |
| #define | Capture_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by Capture_control() for undefined command codes. More... | |
| #define | CAPTURE_CMD_RESERVED Capture_CMD_RESERVED |
| #define | CAPTURE_STATUS_RESERVED Capture_STATUS_RESERVED |
| #define | CAPTURE_STATUS_SUCCESS Capture_STATUS_SUCCESS |
| #define | CAPTURE_STATUS_ERROR Capture_STATUS_ERROR |
| #define | CAPTURE_STATUS_UNDEFINEDCMD Capture_STATUS_UNDEFINEDCMD |
| #define | CAPTURE_MODE_RISING_RISING Capture_RISING_EDGE |
| #define | CAPTURE_MODE_FALLING_FALLING Capture_FALLING_EDGE |
| #define | CAPTURE_MODE_ANY_EDGE Capture_ANY_EDGE |
| #define | CAPTURE_PERIOD_US Capture_PERIOD_US |
| #define | CAPTURE_PERIOD_HZ Capture_PERIOD_HZ |
| #define | CAPTURE_PERIOD_COUNTS Capture_PERIOD_COUNTS |
| #define | Capture_Period_Unit Capture_PeriodUnits |
Typedefs | |
| typedef struct Capture_Config_ * | Capture_Handle |
| A handle that is returned from a Capture_open() call. More... | |
| typedef enum Capture_Mode_ | Capture_Mode |
| Capture mode settings. More... | |
| typedef enum Capture_PeriodUnits_ | Capture_PeriodUnits |
| Capture period unit enum. More... | |
| typedef void(* | Capture_CallBackFxn) (Capture_Handle handle, uint32_t interval) |
| Capture callback function. More... | |
| typedef struct Capture_Params_ | Capture_Params |
| Capture Parameters. More... | |
| typedef void(* | Capture_CloseFxn) (Capture_Handle handle) |
| A function pointer to a driver specific implementation of Capture_close(). More... | |
| typedef int_fast16_t(* | Capture_ControlFxn) (Capture_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of Capture_control(). More... | |
| typedef void(* | Capture_InitFxn) (Capture_Handle handle) |
| A function pointer to a driver specific implementation of Capture_init(). More... | |
| typedef Capture_Handle(* | Capture_OpenFxn) (Capture_Handle handle, Capture_Params *params) |
| A function pointer to a driver specific implementation of Capture_open(). More... | |
| typedef int32_t(* | Capture_StartFxn) (Capture_Handle handle) |
| A function pointer to a driver specific implementation of Capture_start(). More... | |
| typedef void(* | Capture_StopFxn) (Capture_Handle handle) |
| A function pointer to a driver specific implementation of Capture_stop(). More... | |
| typedef struct Capture_FxnTable_ | Capture_FxnTable |
| The definition of a capture function table that contains the required set of functions to control a specific capture driver implementation. More... | |
| typedef struct Capture_Config_ | Capture_Config |
| Capture Global configuration. More... | |
Enumerations | |
| enum | Capture_Mode_ { Capture_RISING_EDGE, Capture_FALLING_EDGE, Capture_ANY_EDGE } |
| Capture mode settings. More... | |
| enum | Capture_PeriodUnits_ { Capture_PERIOD_US, Capture_PERIOD_HZ, Capture_PERIOD_COUNTS } |
| Capture period unit enum. More... | |
Functions | |
| void | Capture_close (Capture_Handle handle) |
| Function to close a capture driver instance. The corresponding timer peripheral to Capture_handle becomes an available resource. More... | |
| int_fast16_t | Capture_control (Capture_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given Capture_Handle. More... | |
| void | Capture_init (void) |
| Function to initialize the capture driver. This function will go through all available hardware resources and mark them as "available". More... | |
| Capture_Handle | Capture_open (uint_least8_t index, Capture_Params *params) |
| Function to open a given capture instance specified by the index argument. The Capture_Params specifies which mode the capture instance will operate. This function takes care of capture resource allocation. If the particular timer hardware is available to use, the capture driver acquires it and returns a Capture_Handle. More... | |
| void | Capture_Params_init (Capture_Params *params) |
| Function to initialize the Capture_Params struct to its defaults. More... | |
| int32_t | Capture_start (Capture_Handle handle) |
| Function to start the capture instance. More... | |
| void | Capture_stop (Capture_Handle handle) |
| Function to stop a capture instance. If the capture instance is already stopped, this function has no effect. More... | |
| #define Capture_CMD_RESERVED (32) |
Common Capture_control command code reservation offset. Capture driver implementations should offset command codes with Capture_CMD_RESERVED growing positively.
Example implementation specific command codes:
| #define Capture_STATUS_RESERVED (-32) |
Common Capture_control status code reservation offset. Capture driver implementations should offset status codes with Capture_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
| #define Capture_STATUS_SUCCESS (0) |
Successful status code.
| #define Capture_STATUS_ERROR (-1) |
Generic error status code.
| #define Capture_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Capture_control() for undefined command codes.
Capture_control() returns Capture_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
| #define CAPTURE_CMD_RESERVED Capture_CMD_RESERVED |
| #define CAPTURE_STATUS_RESERVED Capture_STATUS_RESERVED |
| #define CAPTURE_STATUS_SUCCESS Capture_STATUS_SUCCESS |
| #define CAPTURE_STATUS_ERROR Capture_STATUS_ERROR |
| #define CAPTURE_STATUS_UNDEFINEDCMD Capture_STATUS_UNDEFINEDCMD |
| #define CAPTURE_MODE_RISING_RISING Capture_RISING_EDGE |
| #define CAPTURE_MODE_FALLING_FALLING Capture_FALLING_EDGE |
| #define CAPTURE_MODE_ANY_EDGE Capture_ANY_EDGE |
| #define CAPTURE_PERIOD_US Capture_PERIOD_US |
| #define CAPTURE_PERIOD_HZ Capture_PERIOD_HZ |
| #define CAPTURE_PERIOD_COUNTS Capture_PERIOD_COUNTS |
| #define Capture_Period_Unit Capture_PeriodUnits |
| typedef struct Capture_Config_* Capture_Handle |
A handle that is returned from a Capture_open() call.
| typedef enum Capture_Mode_ Capture_Mode |
Capture mode settings.
This enum defines the capture modes that may be specified in Capture_Params.
| typedef enum Capture_PeriodUnits_ Capture_PeriodUnits |
Capture period unit enum.
This enum defines the units that may be specified for the period in Capture_Params.
| typedef void(* Capture_CallBackFxn) (Capture_Handle handle, uint32_t interval) |
Capture callback function.
User definable callback function prototype. The capture driver will call the defined function and pass in the capture driver's handle and the pointer to the user-specified the argument.
| handle | Capture_Handle |
| interval | Interval of two triggering edges in Capture_PeriodUnits |
| typedef struct Capture_Params_ Capture_Params |
Capture Parameters.
Capture parameters are used by the Capture_open() call. Default values for these parameters are set using Capture_Params_init().
| typedef void(* Capture_CloseFxn) (Capture_Handle handle) |
A function pointer to a driver specific implementation of Capture_close().
| typedef int_fast16_t(* Capture_ControlFxn) (Capture_Handle handle, uint_fast16_t cmd, void *arg) |
A function pointer to a driver specific implementation of Capture_control().
| typedef void(* Capture_InitFxn) (Capture_Handle handle) |
A function pointer to a driver specific implementation of Capture_init().
| typedef Capture_Handle(* Capture_OpenFxn) (Capture_Handle handle, Capture_Params *params) |
A function pointer to a driver specific implementation of Capture_open().
| typedef int32_t(* Capture_StartFxn) (Capture_Handle handle) |
A function pointer to a driver specific implementation of Capture_start().
| typedef void(* Capture_StopFxn) (Capture_Handle handle) |
A function pointer to a driver specific implementation of Capture_stop().
| typedef struct Capture_FxnTable_ Capture_FxnTable |
The definition of a capture function table that contains the required set of functions to control a specific capture driver implementation.
| typedef struct Capture_Config_ Capture_Config |
Capture Global configuration.
The Capture_Config structure contains a set of pointers used to characterize the capture driver implementation.
This structure needs to be defined before calling Capture_init() and it must not be changed thereafter.
| enum Capture_Mode_ |
Capture mode settings.
This enum defines the capture modes that may be specified in Capture_Params.
| Enumerator | |
|---|---|
| Capture_RISING_EDGE | Capture is triggered on rising edges. |
| Capture_FALLING_EDGE | Capture is triggered on falling edges. |
| Capture_ANY_EDGE | Capture is triggered on both rising and falling edges. |
| enum Capture_PeriodUnits_ |
Capture period unit enum.
This enum defines the units that may be specified for the period in Capture_Params.
| void Capture_close | ( | Capture_Handle | handle | ) |
Function to close a capture driver instance. The corresponding timer peripheral to Capture_handle becomes an available resource.
| handle | A Capture_Handle returned from Capture_open(). |
| int_fast16_t Capture_control | ( | Capture_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given Capture_Handle.
| handle | A Capture_Handle returned from Capture_open(). |
| cmd | A command value defined by the driver specific implementation. |
| arg | A pointer to an optional R/W (read/write) argument that is accompanied with cmd. |
| void Capture_init | ( | void | ) |
Function to initialize the capture driver. This function will go through all available hardware resources and mark them as "available".
| Capture_Handle Capture_open | ( | uint_least8_t | index, |
| Capture_Params * | params | ||
| ) |
Function to open a given capture instance specified by the index argument. The Capture_Params specifies which mode the capture instance will operate. This function takes care of capture resource allocation. If the particular timer hardware is available to use, the capture driver acquires it and returns a Capture_Handle.
| index | Logical instance number for the capture indexed into the Capture_config table. |
| params | Pointer to a parameter block. Cannot be NULL. |
| void Capture_Params_init | ( | Capture_Params * | params | ) |
Function to initialize the Capture_Params struct to its defaults.
| params | An pointer to Capture_Params structure for initialization. |
Defaults values are: callbackFxn = NULL mode = Capture_RISING_EDGE periodUnit = Capture_PERIOD_COUNTS
| int32_t Capture_start | ( | Capture_Handle | handle | ) |
Function to start the capture instance.
| handle | A Capture_Handle returned from Capture_open(). |
| void Capture_stop | ( | Capture_Handle | handle | ) |
Function to stop a capture instance. If the capture instance is already stopped, this function has no effect.
| handle | A Capture_Handle returned from Capture_open(). |