SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.27
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_i16 | LenOrPadding |
_u8 | Sd |
_u8 | FamilyAndFlags |
_u16 | Port |
_u8 | Address [6] |
Definition at line 783 of file protocol.h.
_u8 Address[6] |
Definition at line 789 of file protocol.h.
_u8 FamilyAndFlags |
Definition at line 787 of file protocol.h.
_i16 LenOrPadding |
Definition at line 785 of file protocol.h.
_u16 Port |
Definition at line 788 of file protocol.h.
_u8 Sd |
Definition at line 786 of file protocol.h.