![]() |
SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.27
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | Ip [4] |
_u8 | IpMask [4] |
_u8 | IpGateway [4] |
_u8 | IpDnsServer [4] |
_u8 | IpStart [4] |
_u8 | IpEnd [4] |
Definition at line 684 of file protocol.h.
_u8 Ip[4] |
Definition at line 686 of file protocol.h.
_u8 IpDnsServer[4] |
Definition at line 689 of file protocol.h.
_u8 IpEnd[4] |
Definition at line 691 of file protocol.h.
_u8 IpGateway[4] |
Definition at line 688 of file protocol.h.
_u8 IpMask[4] |
Definition at line 687 of file protocol.h.
_u8 IpStart[4] |
Definition at line 690 of file protocol.h.