![]() |
SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.27
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u16 | Status |
_u16 | Padding |
_u32 | Ip0 |
_u32 | Ip1 |
_u32 | Ip2 |
_u32 | Ip3 |
Definition at line 986 of file protocol.h.
_u32 Ip0 |
Definition at line 990 of file protocol.h.
_u32 Ip1 |
Definition at line 991 of file protocol.h.
_u32 Ip2 |
Definition at line 992 of file protocol.h.
_u32 Ip3 |
Definition at line 993 of file protocol.h.
_u16 Padding |
Definition at line 989 of file protocol.h.
_u16 Status |
Definition at line 988 of file protocol.h.