SimpleLink CC3120/CC3220 Host Driver  Version 2.0.1.27
Simplifies the implementation of Internet connectivity
_SlCmdCtrl_t Struct Reference

Data Fields

_SlOpcode_t Opcode
 
_SlArgSize_t TxDescLen
 
_SlArgSize_t RxDescLen
 

Detailed Description

Definition at line 179 of file driver.h.

Field Documentation

§ Opcode

_SlOpcode_t Opcode

Definition at line 181 of file driver.h.

§ RxDescLen

_SlArgSize_t RxDescLen

Definition at line 183 of file driver.h.

§ TxDescLen

_SlArgSize_t TxDescLen

Definition at line 182 of file driver.h.


The documentation for this struct was generated from the following file: