SimpleLink CC3120/CC3220 Host Driver  Version 2.0.1.27
Simplifies the implementation of Internet connectivity
_SlActionLookup_t Struct Reference

Data Fields

_u8 ActionID
 
_u16 ActionAsyncOpcode
 
_SlSpawnEntryFunc_t AsyncEventHandler
 

Detailed Description

Definition at line 254 of file driver.h.

Field Documentation

§ ActionAsyncOpcode

_u16 ActionAsyncOpcode

Definition at line 257 of file driver.h.

§ ActionID

_u8 ActionID

Definition at line 256 of file driver.h.

§ AsyncEventHandler

_SlSpawnEntryFunc_t AsyncEventHandler

Definition at line 258 of file driver.h.


The documentation for this struct was generated from the following file: