SimpleLink CC3220/CC3120 Host Driver  Version 2.0.1.15
Simplifies the implementation of Internet connectivity
NetCfg

Controls the configuration of the device addresses (i.e. IP and MAC addresses) More...

Functions

_i16 sl_NetCfgSet (const _u16 ConfigId, const _u16 ConfigOpt, const _u16 ConfigLen, const _u8 *pValues)
 Setting network configurations. More...
 
_i16 sl_NetCfgGet (const _u16 ConfigId, _u16 *pConfigOpt, _u16 *pConfigLen, _u8 *pValues)
 Getting network configurations. More...
 

Enumerations

enum  SlNetCfg_e {
  SL_NETCFG_MAC_ADDRESS_SET = 1,
  SL_NETCFG_MAC_ADDRESS_GET = 2,
  SL_NETCFG_AP_STATIONS_NUM_CONNECTED = 3,
  SL_NETCFG_AP_STATIONS_INFO_LIST = 4,
  SL_NETCFG_AP_STATION_DISCONNECT = 5,
  SL_NETCFG_IF = 6,
  SL_NETCFG_IPV4_STA_ADDR_MODE = 7,
  SL_NETCFG_IPV4_AP_ADDR_MODE = 8,
  SL_NETCFG_IPV6_ADDR_LOCAL = 9,
  SL_NETCFG_IPV6_ADDR_GLOBAL = 10,
  SL_NETCFG_IPV4_DHCP_CLIENT = 11,
  SL_NETCFG_IPV4_DNS_CLIENT = 12,
  MAX_SETTINGS = 0xFF
}
 
enum  SlNetCfgIpv4DhcpClientState_e {
  SL_NETCFG_DHCP_CLIENT_UNKNOWN = 0,
  SL_NETCFG_DHCP_CLIENT_DISABLED,
  SL_NETCFG_DHCP_CLIENT_ENABLED,
  SL_NETCFG_DHCP_CLIENT_BOUND,
  SL_NETCFG_DHCP_CLIENT_RENEW,
  SL_NETCFG_DHCP_CLIENT_REBIND
}
 
enum  SlNetCfgDhcpOption_e {
  SL_NETCFG_DHCP_OPT_DISABLE_LLA = 0x2,
  SL_NETCFG_DHCP_OPT_RELEASE_IP_BEFORE_DISCONNECT = 0x4,
  MAX_SL_NETCFG_DHCP_OPT = 0xFF
}
 

Detailed Description

Controls the configuration of the device addresses (i.e. IP and MAC addresses)

Function Documentation

_i16 sl_NetCfgGet ( const _u16  ConfigId,
_u16 *  pConfigOpt,
_u16 *  pConfigLen,
_u8 *  pValues 
)

Getting network configurations.

Parameters
[in]ConfigIdConfiguration id
[out]pConfigOptGet configurations option
[out]pConfigLenThe length of the allocated memory as input, when the function complete, the value of this parameter would be the len that actually read from the device.
If the device return length that is longer from the input value, the function will cut the end of the returned structure and will return ESMALLBUF
[out]pValues- get configurations values
Returns
Zero on success, or -1 on failure
See also
sl_NetCfgSet
Note
Warning
Examples
  • SL_NETCFG_MAC_ADDRESS_GET:
    Get the device MAC address. The returned MAC address is taken from FileSystem first. If the MAC address was not set by SL_MAC_ADDRESS_SET, the default MAC address is retrieved from HW.
    1 _u8 macAddressVal[SL_MAC_ADDR_LEN];
    2 _u16 macAddressLen = SL_MAC_ADDR_LEN;
    3 _u16 ConfigOpt = 0;
    4 sl_NetCfgGet(SL_NETCFG_MAC_ADDRESS_GET,&ConfigOpt,&macAddressLen,(_u8 *)macAddressVal);

  • SL_NETCFG_IPV4_STA_ADDR_MODE:
    Get IP address from WLAN station or P2P client. A DHCP flag is returned to indicate if the IP address is static or from DHCP.
    1 _u16 len = sizeof(SlNetCfgIpV4Args_t);
    2 _u16 ConfigOpt = 0; //return value could be one of the following: SL_NETCFG_ADDR_DHCP / SL_NETCFG_ADDR_DHCP_LLA / SL_NETCFG_ADDR_STATIC
    3 SlNetCfgIpV4Args_t ipV4 = {0};
    4 sl_NetCfgGet(SL_NETCFG_IPV4_STA_ADDR_MODE,&ConfigOpt,&len,(_u8 *)&ipV4);
    5 
    6 printf("DHCP is %s IP %d.%d.%d.%d MASK %d.%d.%d.%d GW %d.%d.%d.%d DNS %d.%d.%d.%d\n",
    7  (ConfigOpt == SL_NETCFG_ADDR_DHCP) ? "ON" : "OFF",
    8  SL_IPV4_BYTE(ipV4.Ip,3),SL_IPV4_BYTE(ipV4.Ip,2),SL_IPV4_BYTE(ipV4.Ip,1),SL_IPV4_BYTE(ipV4.Ip,0),
    9  SL_IPV4_BYTE(ipV4.IpMask,3),SL_IPV4_BYTE(ipV4.IpMask,2),SL_IPV4_BYTE(ipV4.IpMask,1),SL_IPV4_BYTE(ipV4.IpMask,0),
    10  SL_IPV4_BYTE(ipV4.IpGateway,3),SL_IPV4_BYTE(ipV4.IpGateway,2),SL_IPV4_BYTE(ipV4.IpGateway,1),SL_IPV4_BYTE(ipV4.IpGateway,0),
    11  SL_IPV4_BYTE(ipV4.IpDnsServer,3),SL_IPV4_BYTE(ipV4.IpDnsServer,2),SL_IPV4_BYTE(ipV4.IpDnsServer,1),SL_IPV4_BYTE(ipV4.IpDnsServer,0));

  • SL_NETCFG_IPV4_AP_ADDR_MODE:
    Get static IP address for AP or P2P go.
    1 _u16 len = sizeof(SlNetCfgIpV4Args_t);
    2 _u16 ConfigOpt = 0; //return value could be one of the following: SL_NETCFG_ADDR_DHCP / SL_NETCFG_ADDR_DHCP_LLA / SL_NETCFG_ADDR_STATIC
    3 SlNetCfgIpV4Args_t ipV4 = {0};
    4 sl_NetCfgGet(SL_NETCFG_IPV4_AP_ADDR_MODE,&ConfigOpt,&len,(_u8 *)&ipV4);
    5 
    6 printf("DHCP is %s IP %d.%d.%d.%d MASK %d.%d.%d.%d GW %d.%d.%d.%d DNS %d.%d.%d.%d\n",
    7  (ConfigOpt == SL_NETCFG_ADDR_DHCP) ? "ON" : "OFF",
    8  SL_IPV4_BYTE(ipV4.Ip,3),SL_IPV4_BYTE(ipV4.Ip,2),SL_IPV4_BYTE(ipV4.Ip,1),SL_IPV4_BYTE(ipV4.Ip,0),
    9  SL_IPV4_BYTE(ipV4.IpMask,3),SL_IPV4_BYTE(ipV4.IpMask,2),SL_IPV4_BYTE(ipV4.IpMask,1),SL_IPV4_BYTE(ipV4.IpMask,0),
    10  SL_IPV4_BYTE(ipV4.IpGateway,3),SL_IPV4_BYTE(ipV4.IpGateway,2),SL_IPV4_BYTE(ipV4.IpGateway,1),SL_IPV4_BYTE(ipV4.IpGateway,0),
    11  SL_IPV4_BYTE(ipV4.IpDnsServer,3),SL_IPV4_BYTE(ipV4.IpDnsServer,2),SL_IPV4_BYTE(ipV4.IpDnsServer,1),SL_IPV4_BYTE(ipV4.IpDnsServer,0));

  • SL_NETCFG_IF:
    Get interface bitmap
    1 _u16 len;
    2 _u32 IfBitmap;
    3 len = sizeof(IfBitmap);
    4 sl_NetCfgGet(SL_NETCFG_IF,NULL,&len,(_u8 *)&IfBitmap);

  • SL_NETCFG_IPV6_ADDR_LOCAL:
    Get IPV6 Local address (ipV6.ipV6IsValid holds the address status. 1=Valid, ipv6 DAD completed and address is valid for use)
    1 SlNetCfgIpV6Args_t ipV6;
    2 _u16 len = sizeof(SlNetCfgIpV6Args_t);
    3 _u16 ConfigOpt = 0; //return value could be one of the following: SL_NETCFG_ADDR_STATIC / SL_NETCFG_ADDR_STATELESS / SL_NETCFG_ADDR_STATEFUL
    4 
    5 sl_NetCfgGet(SL_NETCFG_IPV6_ADDR_LOCAL,&ConfigOpt,&len,(_u8 *)&ipV6);
    6 if (SL_IS_IPV6_ADDR_VALID(ipV6.IpV6Flags))
    7 {
    8  printf("Ipv6 Local Address is valid: %8x:%8x:%8x:%8x\n", ipV6.Ip[0],ipV6.Ip[0],ipV6.Ip[0],ipV6.Ip[0]);
    9 }
    10 else
    11 {
    12  printf("Ipv6 Local Address is not valid, wait for DAD to complete or configure a different address");
    13 }

  • SL_NETCFG_IPV6_ADDR_GLOBAL:
    Get IPV6 Global address (ipV6.ipV6IsValid holds the address status. 1=Valid, ipv6 DAD completed and address is valid for use)
    1 SlNetCfgIpV6Args_t ipV6;
    2 _u16 len = sizeof(SlNetCfgIpV6Args_t);
    3 _u16 ConfigOpt = 0; //return value could be one of the following: SL_NETCFG_ADDR_STATIC / SL_NETCFG_ADDR_STATEFUL
    4 
    5 if (SL_IS_IPV6_ADDR_VALID(ipV6.IpV6Flags))
    6 {
    7  printf("Ipv6 Global Address is valid: %8x:%8x:%8x:%8x\n", ipV6.Ip[0],ipV6.Ip[0],ipV6.Ip[0],ipV6.Ip[0]);
    8 }
    9 else
    10 {
    11  printf("Ipv6 Global Address is not valid, wait for DAD to complete or configure a different address");
    12 }

  • SL_NETCFG_AP_STATIONS_NUM_CONNECTED:
    Get AP numbber of connected stations.
    1 _u8 num_ap_connected_sta;
    2 _u16 len = sizeof(num_ap_connected_sta);
    3 sl_NetCfgGet(SL_NETCFG_AP_STATIONS_NUM_CONNECTED, NULL, &len, &num_ap_connected_sta);
    4 printf("AP number of connected stations = %d\n", num_ap_connected_sta);

  • SL_NETCFG_AP_STATIONS_INFO_LIST:
    Get AP full list of connected stationss.
    1 SlNetCfgStaInfo_t ApStaList[4];
    2 _u16 sta_info_len;
    3 _u16 start_sta_index = 0;
    4 int actual_num_sta;
    5 int i;
    6 
    7 start_sta_index = 0;
    8 sta_info_len = sizeof(ApStaList);
    9 sl_NetCfgGet(SL_NETCFG_AP_STATIONS_INFO_LIST, &start_sta_index, &sta_info_len, (_u8 *)ApStaList);
    10 
    11 actual_num_sta = sta_info_len / sizeof(SlNetCfgStaInfo_t);
    12 printf("-Print SL_NETCFG_AP_STATIONS_INFO_LIST actual num_stations = %d (upon sta_info_len = %d)\n", actual_num_sta, sta_info_len);
    13 
    14 for (i=0; i<actual_num_sta; i++)
    15 {
    16  SlNetCfgStaInfo_t *staInfo = &ApStaList[i];
    17  printf(" Ap Station %d is connected\n", i);
    18  printf(" NAME: %s\n", staInfo->Name);
    19  printf(" MAC: %02x:%02x:%02x:%02x:%02x:%02x\n", staInfo->MacAddr[0], staInfo->MacAddr[1], staInfo->MacAddr[2], staInfo->MacAddr[3], staInfo->MacAddr[4], staInfo->MacAddr[5]);
    20  printf(" IP: %d.%d.%d.%d\n", SL_IPV4_BYTE(staInfo->Ip,3), SL_IPV4_BYTE(staInfo->Ip,2), SL_IPV4_BYTE(staInfo->Ip,1), SL_IPV4_BYTE(staInfo->Ip,0));
    21 }

  • SL_NETCFG_IPV4_DNS_CLIENT:
    Set secondary DNS address (DHCP and static configuration)
    1 _u16 ConfigOpt = 0;
    2 _i32 Status;
    3 _u16 pConfigLen = sizeof(SlNetCfgIpV4DnsClientArgs_t);
    4 SlNetCfgIpV4DnsClientArgs_t DnsOpt;
    5 Status = sl_NetCfgGet(SL_NETCFG_IPV4_DNS_CLIENT,&ConfigOpt,&pConfigLen,&DnsOpt);
    6 if( Status )
    7 {
    8  // error
    9 }
  • SL_NETCFG_IPV4_DHCP_CLIENT:
    Get DHCP Client info
    1 _u16 ConfigOpt = 0;
    2 _u16 pConfigLen = sizeof(SlNetCfgIpv4DhcpClient_t);
    3 SlNetCfgIpv4DhcpClient_t dhcpCl;
    4 SlNetCfgIpV4Args_t ipV4 = {0};
    5 
    6 ret = sl_NetCfgGet(SL_NETCFG_IPV4_DHCP_CLIENT, &ConfigOpt, &pConfigLen, (_u8 *)&dhcpCl);
    7 if(ret < 0)
    8 {
    9  printf("Error = %d\n", ret);
    10 }
_i16 sl_NetCfgSet ( const _u16  ConfigId,
const _u16  ConfigOpt,
const _u16  ConfigLen,
const _u8 *  pValues 
)

Setting network configurations.

Parameters
[in]ConfigIdConfiguration id:
  • SL_NETCFG_IF
  • SL_NETCFG_IPV4_STA_ADDR_MODE
  • SL_NETCFG_IPV6_ADDR_LOCAL
  • SL_NETCFG_IPV6_ADDR_GLOBAL
  • SL_NETCFG_IPV4_AP_ADDR_MODE
  • SL_NETCFG_MAC_ADDRESS_SET
  • SL_NETCFG_AP_STATION_DISCONNECT
[in]ConfigOptConfigurations option:
  • SL_NETCFG_IF_STATE
  • SL_NETCFG_ADDR_DHCP
  • SL_NETCFG_ADDR_DHCP_LLA
  • SL_NETCFG_ADDR_RELEASE_IP
  • SL_NETCFG_ADDR_STATIC
  • SL_NETCFG_ADDR_STATELESS
  • SL_NETCFG_ADDR_STATEFUL
  • SL_NETCFG_ADDR_RELEASE_IP_SET
  • SL_NETCFG_ADDR_RELEASE_IP_OFF
[in]ConfigLenConfigurations len
[in]pValuesConfigurations values
Persistent
Reset:
  • SL_IPV4_AP_P2P_GO_STATIC_ENABLE
  • SL_NETCFG_MAC_ADDRESS_SET
Non- Persistent:
  • SL_NETCFG_AP_STATION_DISCONNECT
System Persistent:
  • SL_NETCFG_IPV4_STA_ADDR_MODE
  • SL_NETCFG_IF_STATE
  • SL_NETCFG_IPV6_ADDR_LOCAL
  • SL_NETCFG_IPV6_ADDR_GLOBAL
Returns
Zero on success, or -1 for failure
See also
sl_NetCfgGet
Note
Warning
Examples
  • SL_NETCFG_MAC_ADDRESS_SET:
    Setting MAC address to the Device. The new MAC address will override the default MAC address and it be saved in the FileSystem. Requires restarting the device for updating this setting.
    1 _u8 MAC_Address[6];
    2 MAC_Address[0] = 0x8;
    3 MAC_Address[1] = 0x0;
    4 MAC_Address[2] = 0x28;
    5 MAC_Address[3] = 0x22;
    6 MAC_Address[4] = 0x69;
    7 MAC_Address[5] = 0x31;
    8 sl_NetCfgSet(SL_NETCFG_MAC_ADDRESS_SET,1,SL_MAC_ADDR_LEN,(_u8 *)MAC_Address);
    9 sl_Stop(0);
    10 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV4_STA_ADDR_MODE
    :
  • SL_NETCFG_ADDR_STATIC:
    Setting a static IP address to the device working in STA mode or P2P client. The IP address will be stored in the FileSystem.
    1 SlNetCfgIpV4Args_t ipV4;
    2 ipV4.Ip = (_u32)SL_IPV4_VAL(10,1,1,201); // _u32 IP address
    3 ipV4.IpMask = (_u32)SL_IPV4_VAL(255,255,255,0); // _u32 Subnet mask for this STA/P2P
    4 ipV4.IpGateway = (_u32)SL_IPV4_VAL(10,1,1,1); // _u32 Default gateway address
    5 ipV4.IpDnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
    6 
    7 sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV4Args_t),(_u8 *)&ipV4);
    8 sl_Stop(0);
    9 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_ADDR_DHCP:
    Setting IP address by DHCP to FileSystem using WLAN sta mode or P2P client. This should be done once if using Serial Flash. This is the system's default mode for acquiring an IP address after WLAN connection.
    1 sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_DHCP,0,0);
    2 sl_Stop(0);
    3 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_ADDR_DHCP_LLA:
    Setting DHCP LLA will runs LLA mechanism in case DHCP fails to acquire an address SL_NETCFG_DHCP_OPT_RELEASE_IP_BEFORE_DISCONNECT - If set, enables sending a DHCP release frame to the server if user issues a WLAN disconnect command.
    1 sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_DHCP_LLA,0,0);
    2 sl_Stop(0);
    3 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_ADDR_RELEASE_IP_SET:
    Setting release ip before disconnect enables sending a DHCP release frame to the server if user issues a WLAN disconnect command.
    1 sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_RELEASE_IP_SET,0,0);
    2 sl_Stop(0);
    3 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_ADDR_RELEASE_IP_OFF:
    Setting release ip before disconnect disables sending a DHCP release frame to the server if user issues a WLAN disconnect command.
    1 sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_RELEASE_IP_OFF,0,0);
    2 sl_Stop(0);
    3 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV4_AP_ADDR_MODE:
    Setting a static IP address to the device working in AP mode or P2P go. The IP address will be stored in the FileSystem. Requires restart.
    1 SlNetCfgIpV4Args_t ipV4;
    2 ipV4.Ip = (_u32)SL_IPV4_VAL(10,1,1,201); // _u32 IP address
    3 ipV4.IpMask = (_u32)SL_IPV4_VAL(255,255,255,0); // _u32 Subnet mask for this AP/P2P
    4 ipV4.IpGateway = (_u32)SL_IPV4_VAL(10,1,1,1); // _u32 Default gateway address
    5 ipV4.IpDnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
    6 
    7 sl_NetCfgSet(SL_NETCFG_IPV4_AP_ADDR_MODE,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV4Args_t),(_u8 *)&ipV4);
    8 sl_Stop(0);
    9 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IF:
    Enable IPV6 interface - Local or/and Global address (Global could not be enabled without Local)
    1 _u32 IfBitmap = 0;
    2 
    3 IfBitmap = SL_NETCFG_IF_IPV6_STA_LOCAL | SL_NETCFG_IF_IPV6_STA_GLOBAL;
    4 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    5 sl_Stop(0);
    6 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV6_ADDR_LOCAL:
    Setting a IPv6 Local static address to the device working in STA mode. The IP address will be stored in the FileSystem. Requires restart.
    1 SlNetCfgIpV6Args_t ipV6;
    2 _u32 IfBitmap = 0;
    3 
    4 IfBitmap = SL_NETCFG_IF_IPV6_STA_LOCAL;
    5 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    6 
    7 ipV6.Ip[0] = 0xfe800000;
    8 ipV6.Ip[1] = 0x00000000;
    9 ipV6.Ip[2] = 0x00004040;
    10 ipV6.Ip[3] = 0x0000ce65;
    11 
    12 sl_NetCfgSet(SL_NETCFG_IPV6_ADDR_LOCAL,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV6Args_t),(_u8 *)&ipV6);
    13 sl_Stop(0);
    14 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV6_ADDR_LOCAL:
    Setting a IPv6 Local stateless address to the device working in STA mode. The IP address will be stored in the FileSystem. Requires restart.
    1 _u32 IfBitmap = 0;
    2 IfBitmap = SL_NETCFG_IF_IPV6_STA_LOCAL;
    3 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    4 sl_NetCfgSet(SL_NETCFG_IPV6_ADDR_LOCAL,SL_NETCFG_ADDR_STATELESS,0,0);
    5 sl_Stop(0);
    6 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV6_ADDR_LOCAL:
    Setting a IPv6 Local statefull address to the device working in STA mode. The IP address will be stored in the FileSystem. Requires restart.
    1 _u32 IfBitmap = 0;
    2 
    3 IfBitmap = SL_NETCFG_IF_IPV6_STA_LOCAL;
    4 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    5 sl_NetCfgSet(SL_NETCFG_IPV6_ADDR_LOCAL,SL_NETCFG_ADDR_STATEFUL,0,0);
    6 sl_Stop(0);
    7 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV6_ADDR_GLOBAL:
    Setting a IPv6 Global static address to the device working in STA mode. The IP address will be stored in the FileSystem. Requires restart.
    1 SlNetCfgIpV6Args_t ipV6;
    2 _u32 IfBitmap = 0;
    3 
    4 ipV6.Ip[0] = 0xfe80;
    5 ipV6.Ip[1] = 0x03a;
    6 ipV6.Ip[2] = 0x4040;
    7 ipV6.Ip[3] = 0xce65;
    8 
    9 ipV6.IpDnsServer[0] = 0xa780;
    10 ipV6.IpDnsServer[1] = 0x65e;
    11 ipV6.IpDnsServer[2] = 0x8;
    12 ipV6.IpDnsServer[3] = 0xce00;
    13 
    14 IfBitmap = SL_NETCFG_IF_IPV6_STA_GLOBAL;
    15 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    16 sl_NetCfgSet(SL_NETCFG_IPV6_ADDR_GLOBAL,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV6Args_t),(_u8 *)&ipV6);
    17 sl_Stop(0);
    18 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_IPV6_ADDR_GLOBAL:
    Setting a IPv6 Global statefull address to the device working in STA mode. The IP address will be stored in the FileSystem. Requires restart.
    1 _u32 IfBitmap = 0;
    2 IfBitmap = SL_NETCFG_IF_IPV6_STA_GLOBAL;
    3 sl_NetCfgSet(SL_NETCFG_IF,SL_NETCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
    4 sl_NetCfgSet(SL_NETCFG_IPV6_ADDR_GLOBAL,SL_NETCFG_ADDR_STATEFUL,0,0);
    5 sl_Stop(0);
    6 sl_Start(NULL,NULL,NULL);

  • SL_NETCFG_AP_STATION_DISCONNECT:
    Disconnet AP station by mac address. The AP connected stations list can be read by sl_NetCfgGet with options: SL_AP_STATIONS_NUM_CONNECTED, SL_AP_STATIONS_INFO_LIST
    1 _u8 ap_sta_mac[6] = { 0x00, 0x22, 0x33, 0x44, 0x55, 0x66 };
    2 sl_NetCfgSet(SL_NETCFG_AP_STATION_DISCONNECT,1,SL_MAC_ADDR_LEN,(_u8 *)ap_sta_mac);

  • SL_NETCFG_IPV4_DNS_CLIENT:
    Set secondary DNS address (DHCP and static configuration) not persistent
    1 _i32 Status;
    2 SlNetCfgIpV4DnsClientArgs_t DnsOpt;
    3 DnsOpt.DnsSecondServerAddr = SL_IPV4_VAL(8,8,8,8); ;
    4 Status = sl_NetCfgSet(SL_NETCFG_IPV4_DNS_CLIENT,0,sizeof(SlNetCfgIpV4DnsClientArgs_t),(unsigned char *)&DnsOpt);
    5 if( Status )
    6 {
    7  // error
    8 }

Data Structure Documentation

struct SlNetCfgIpV4DnsClientArgs_t

Definition at line 103 of file netcfg.h.

Data Fields
_u32 DnsSecondServerAddr
struct SlNetCfgIpv4DhcpClient_t

Definition at line 109 of file netcfg.h.

Data Fields
_u32 DhcpServer
_u8 DhcpState
_u32 Dns[2]
_u32 Gateway
_u32 Ip
_u32 LeaseTime
_u32 Mask
_u8 Reserved[3]
_u32 TimeToRenew
struct SlNetCfgIpV4Args_t

Definition at line 141 of file netcfg.h.

Data Fields
_u32 Ip
_u32 IpDnsServer
_u32 IpGateway
_u32 IpMask
struct SlNetCfgIpV6Args_t

Definition at line 150 of file netcfg.h.

Data Fields
_u32 Ip[4]
_u32 IpDnsServer[4]
_u32 IpV6Flags
struct SlNetCfgStaInfo_t

Definition at line 162 of file netcfg.h.

Data Fields
_u32 Ip
_u8 MacAddr[6]
_u8 Name[32]
_u16 Status