EDMA3_RM_Obj Struct Reference

EDMA3 Hardware Instance Configuration Structure. More...

#include <edma3resmgr.h>

Data Fields

unsigned int phyCtrllerInstId
EDMA3_RM_ObjState state
unsigned int numOpens
EDMA3_RM_GblConfigParams gblCfgParams
 Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information.

Detailed Description

EDMA3 Hardware Instance Configuration Structure.

Used to maintain information of the EDMA3 HW configuration. One such storage exists for each instance of the EDMA 3 HW.


Field Documentation

HW Instance Id of the EDMA3 Controller

EDMA3_RM_ObjState EDMA3_RM_Obj::state

State information of the Resource Manager object

unsigned int EDMA3_RM_Obj::numOpens

Number of active opens of RM Instances

Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information.

This configuration will can be provided by the user at run-time, while calling EDMA3_RM_create().


The documentation for this struct was generated from the following file:

Generated on Fri Jan 28 16:33:51 2011 for EDMA3 Resource Manager by  doxygen 1.6.1