EDMA3_RM_ChBoundResources Struct Reference

EDMA3 Channel-Bound resources. More...

#include <edma3resmgr.h>

Data Fields

int paRAMId
unsigned int tcc

Detailed Description

EDMA3 Channel-Bound resources.

Used to maintain information of the EDMA3 resources (specifically Parameter RAM set and TCC), bound to the particular channel within EDMA3_RM_allocLogicalChannel ().


Field Documentation

PaRAM Set number associated with the particular channel

TCC associated with the particular channel


The documentation for this struct was generated from the following file:

Generated on Fri Jan 28 16:33:50 2011 for EDMA3 Resource Manager by  doxygen 1.6.1