#include <edma3.h>
Data Fields | |
unsigned int | phyCtrllerInstId |
EDMA3_DRV_ObjState | state |
unsigned int | numOpens |
EDMA3_DRV_GblConfigParams | gblCfgParams |
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information. |
Used to maintain information of the EDMA3 HW configuration thoughout the lifetime of the EDMA3 Driver Object, one for each EDMA3 hardware instance.
unsigned int EDMA3_DRV_Object::phyCtrllerInstId |
Physical Instance ID of EDMA3 Controller
EDMA3_DRV_ObjState EDMA3_DRV_Object::state |
State information of the EDMA3 Driver object
unsigned int EDMA3_DRV_Object::numOpens |
Number of EDMA3 Driver instances
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information.
This configuration info can be provided by the user at run-time, while calling EDMA3_DRV_create(). If not provided at run-time, this info will be taken from the config file edma3Cfg.c.