#include <edma3resmgr.h>
Data Fields | |
unsigned int | phyCtrllerInstId |
EDMA3_RM_ObjState | state |
unsigned int | numOpens |
EDMA3_RM_GblConfigParams | gblCfgParams |
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information. |
Used to maintain information of the EDMA3 HW configuration. One such storage exists for each instance of the EDMA 3 HW.
unsigned int EDMA3_RM_Obj::phyCtrllerInstId |
HW Instance Id of the EDMA3 Controller
EDMA3_RM_ObjState EDMA3_RM_Obj::state |
State information of the Resource Manager object
unsigned int EDMA3_RM_Obj::numOpens |
Number of active opens of RM Instances
Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information.
This configuration will can be provided by the user at run-time, while calling EDMA3_RM_create().