#include <edma3_rm.h>
Data Fields | |
EDMA3_RM_RegionId | regionId |
unsigned int | isMaster |
EDMA3_RM_InstanceInitConfig * | rmInstInitConfig |
void * | rmSemHandle |
unsigned int | regionInitEnable |
EDMA3_RM_GblErrCallbackParams | gblerrCbParams |
This configuration structure is used to initialize the EDMA3 RM Instance. This configuration information is passed while opening the RM instance.
Shadow Region Identification
unsigned int EDMA3_RM_Param::isMaster |
It tells whether the EDMA3 RM instance is Master or not. Only the shadow region associated with this master instance will receive the EDMA3 interrupts (if enabled).
EDMA3 resources related shadow region specific information. Which all EDMA3 resources are owned and reserved by this particular instance are told in this configuration structure. User can also pass this structure as NULL. In that case, default static configuration would be taken from the platform specific configuration files (part of the Resource Manager), if available.
EDMA3 RM Instance specific semaphore handle. Used to share resources (DMA/QDMA channels, PaRAM Sets, TCCs etc) among different users.
unsigned int EDMA3_RM_Param::regionInitEnable |
Whether initialization of Region Specific Registers is required or not?
Instance wide Global Error callback parameters