#include <edma3_rm.h>
Data Fields | |
volatile unsigned int | opt |
volatile unsigned int | srcAddr |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address. | |
volatile unsigned short | aCnt |
Number of bytes in each Array (ACNT). | |
volatile unsigned short | bCnt |
Number of Arrays in each Frame (BCNT). | |
volatile unsigned int | destAddr |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0. | |
volatile short | srcBIdx |
Index between consec. arrays of a Source Frame (SRCBIDX) If SAM is set to 1 (via channelOptions) then srcInterArrIndex should be an even multiple of 32 bytes. | |
volatile short | destBIdx |
Index between consec. arrays of a Destination Frame (DSTBIDX) If DAM is set to 1 (via channelOptions) then destInterArrIndex should be an even multiple of 32 bytes. | |
volatile unsigned short | linkAddr |
Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking Linking is especially useful for use with ping-pong buffers and circular buffers. | |
volatile unsigned short | bCntReload |
Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers. | |
volatile short | srcCIdx |
Index between consecutive frames of a Source Block (SRCCIDX). | |
volatile short | destCIdx |
Index between consecutive frames of a Dest Block (DSTCIDX). | |
volatile unsigned short | cCnt |
Number of Frames in a block (CCNT). |
This is a mapping of the EDMA3 PaRAM set provided to the user for ease of modification of the individual fields.
volatile unsigned int EDMA3_RM_PaRAMRegs::opt |
OPT field of PaRAM Set