XDAIS
dais-x04
|
Defines the structure that contains macroblock related encoding parameter estimates. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | mbMode |
XDAS_Int32 | QP |
XDAS_Int32 | mvFwdXY |
XDAS_Int32 | mvBwdXY |
Defines the structure that contains macroblock related encoding parameter estimates.
inBufs
parameter to IVIDENC1_Fxns::process() when IVIDENC1_DynamicParams::mbDataFlag is set.XDAS_Int32 IVIDENC1_MbData::mbMode |
MB encoding mode
XDAS_Int32 IVIDENC1_MbData::QP |
QP estimate.
XDAS_Int32 IVIDENC1_MbData::mvFwdXY |
Forward Motion vector estimate.
XDAS_Int32 IVIDENC1_MbData::mvBwdXY |
Backward motion vector estimate.