XDAIS
dais-x04
|
Defines the run time output arguments for all IVIDANALYTICS instance objects. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numTargets |
XDM_Rect | targets [128] |
XDAS_Int32 | numEvents |
XDAS_Int32 | eventId [128] |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM_Date | date |
Defines the run time output arguments for all IVIDANALYTICS instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDANALYTICS_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDANALYTICS_OutArgs::numTargets |
Number of targets detected
XDM_Rect IVIDANALYTICS_OutArgs::targets[128] |
target locations.
numTargets
is zero, the values in this array are undefined. XDAS_Int32 IVIDANALYTICS_OutArgs::numEvents |
Number of events detected
XDAS_Int32 IVIDANALYTICS_OutArgs::eventId[128] |
Zero-terminated array containing the ids of rules fired during the process() call.
numEvents
is zero, the values in this array are undefined. XDAS_Int32 IVIDANALYTICS_OutArgs::extendedError |
Extended error information.
XDM_Date IVIDANALYTICS_OutArgs::date |
Current time.