XDAIS
dais-x04
|
This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <isphenc.h>
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 ISPHENC_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 ISPHENC_DynamicParams::frameSize |
Input frame size in bytes for sample based codecs.
XDAS_Int32 ISPHENC_DynamicParams::bitRate |
Rate selection for multi_rate codecs
XDAS_Int32 ISPHENC_DynamicParams::mode |
Mode selection for multi_mode codecs
XDAS_Int32 ISPHENC_DynamicParams::vadFlag |
VAD_On =1, VAD_OFF = 0
XDAS_Int32 ISPHENC_DynamicParams::noiseSuppressionMode |
0 - OFF, 1 = NS-A, 2 = NS-B etc
XDAS_Int32 ISPHENC_DynamicParams::ttyTddMode |
0 = TTY OFF, 1 = 45.45bauds 2 = 50 bauds
XDAS_Int32 ISPHENC_DynamicParams::dtmfMode |
0 = DTMF_OFF, 1 = DTMF_ON
XDAS_Int32 ISPHENC_DynamicParams::dataTransmit |
1 = ON, 0 = OFF
XDAS_Int32 ISPHENC_DynamicParams::homingMode |
0 - DISABLED; 1 - ENABLED