![]() |
![]() |
XDAIS
dais-x04
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | inputHeight |
XDAS_Int32 | inputWidth |
XDAS_Int32 | refFrameRate |
XDAS_Int32 | targetFrameRate |
XDAS_Int32 | targetBitRate |
XDAS_Int32 | intraFrameInterval |
XDAS_Int32 | generateHeader |
Encode entire access unit or only header. | |
XDAS_Int32 | captureWidth |
XDAS_Int32 | forceFrame |
XDAS_Int32 | interFrameInterval |
XDAS_Int32 | mbDataFlag |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDENC1_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC1_DynamicParams::inputHeight |
Input frame height.
XDAS_Int32 IVIDENC1_DynamicParams::inputWidth |
Input frame width.
XDAS_Int32 IVIDENC1_DynamicParams::refFrameRate |
Reference, or input, frame rate in fps * 1000.
XDAS_Int32 IVIDENC1_DynamicParams::targetFrameRate |
Target frame rate in fps * 1000.
XDAS_Int32 IVIDENC1_DynamicParams::targetBitRate |
Target bit rate in bits per second.
XDAS_Int32 IVIDENC1_DynamicParams::intraFrameInterval |
The number of frames between two I frames. For example, 30.
XDAS_Int32 IVIDENC1_DynamicParams::generateHeader |
Encode entire access unit or only header.
XDAS_Int32 IVIDENC1_DynamicParams::captureWidth |
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
XDAS_Int32 IVIDENC1_DynamicParams::forceFrame |
Force the current (immediate) frame to be encoded as a specific frame type.
XDAS_Int32 IVIDENC1_DynamicParams::interFrameInterval |
Number of B frames between two reference frames; that is, the number of B frames between two P frames or I/P frames. DEFAULT(0).
XDAS_Int32 IVIDENC1_DynamicParams::mbDataFlag |
Flag to indicate that the algorithm should use MB data supplied in additional buffer within inBufs.