![]() |
![]() |
XDAIS
dais-x04
|
Defines instance status parameters. More...
#include <ividdec3.h>
Defines instance status parameters.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDDEC3_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC3_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc IVIDDEC3_Status::data |
Buffer descriptor for data passing.
data.buf
to NULL.XDAS_Int32 IVIDDEC3_Status::maxNumDisplayBufs |
The maximum number of buffers that will be required by the codec.
XDAS_Int32 IVIDDEC3_Status::maxOutArgsDisplayBufs |
The maximum number of display buffers that can be returned via IVIDDEC3_OutArgs.displayBufs.
XDAS_Int32 IVIDDEC3_Status::outputHeight |
Output height in pixels.
XDAS_Int32 IVIDDEC3_Status::outputWidth |
Output width in pixels.
XDAS_Int32 IVIDDEC3_Status::frameRate |
Average frame rate in fps * 1000. For example, if average frame rate is 30 frames per second, this field should be 30000.
XDAS_Int32 IVIDDEC3_Status::bitRate |
Average bit rate, in bits per second.
XDAS_Int32 IVIDDEC3_Status::contentType |
Video content types.
XDAS_Int32 IVIDDEC3_Status::sampleAspectRatioHeight |
Sample aspect ratio height.
XDAS_Int32 IVIDDEC3_Status::sampleAspectRatioWidth |
Sample aspect ratio width.
XDAS_Int32 IVIDDEC3_Status::bitRange |
Full 8 bit, CCIR 601
XDAS_Int32 IVIDDEC3_Status::forceChromaFormat |
Output chroma format.
XDAS_Int32 IVIDDEC3_Status::operatingMode |
Video decoding mode of operation.
XDAS_Int32 IVIDDEC3_Status::frameOrder |
Frame Order
XDAS_Int32 IVIDDEC3_Status::inputDataMode |
Input data mode.
XDAS_Int32 IVIDDEC3_Status::outputDataMode |
Output data mode.
XDM1_AlgBufInfo IVIDDEC3_Status::bufInfo |
Input and output buffer information.
XDAS_Int32 IVIDDEC3_Status::numInputDataUnits |
Number of input slices/rows.
XDAS_Int32 IVIDDEC3_Status::numOutputDataUnits |
Number of output slices/rows.
outputDataMode
, like number of slices/rows/blocks etc.XDAS_Int32 IVIDDEC3_Status::configurationID |
Configuration ID of given codec.
XDAS_Int32 IVIDDEC3_Status::metadataType[3] |
Type of each metadata plane.
IVIDDEC3_DynamicParams IVIDDEC3_Status::decDynamicParams |
Current values of the decoder's dynamic parameters.