![]() |
![]() |
XDAIS
dais-x04
|
Defines the run time output arguments for all IVIDDEC2FRONT instance objects. More...
#include <ividdec2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | bytesConsumed |
Defines the run time output arguments for all IVIDDEC2FRONT instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDDEC2FRONT_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC2FRONT_OutArgs::extendedError |
Extended error information.
XDAS_Int32 IVIDDEC2FRONT_OutArgs::bytesConsumed |
Number of bytes consumed during the process() call.