![]() |
![]() |
XDAIS
dais-x04
|
Defines the creation time parameters for all ISPHENC instance objects. More...
#include <isphenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | frameSize |
XDAS_Int32 | compandingLaw |
XDAS_Int32 | packingType |
XDAS_Int32 | vadSelection |
Defines the creation time parameters for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 ISPHENC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 ISPHENC_Params::frameSize |
Input frame size in bytes for sample based codecs.
XDAS_Int32 ISPHENC_Params::compandingLaw |
Companding Law.
XDAS_Int32 ISPHENC_Params::packingType |
Packing Format Option (for codecs that support multiple packing formats - used for selection, 0, 1, 2...)
XDAS_Int32 ISPHENC_Params::vadSelection |
VAD A/VAD B, VAD 1/ VAD 2 etc