![]() |
![]() |
XDAIS
dais-x04
|
Defines the run time output arguments for all ISPHENC instance objects. More...
#include <isphenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | rate |
XDAS_Int32 | frameType |
XDAS_Int32 | outbufferSize |
Defines the run time output arguments for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 ISPHENC_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 ISPHENC_OutArgs::rate |
Current frame bit rate.
XDAS_Int32 ISPHENC_OutArgs::frameType |
Current frame type.
XDAS_Int32 ISPHENC_OutArgs::outbufferSize |
Output buffer size in bytes.