![]() |
![]() |
XDAIS
dais-x04
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <iimgenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | inputChromaFormat |
XDAS_Int32 | inputHeight |
XDAS_Int32 | inputWidth |
XDAS_Int32 | captureWidth |
XDAS_Int32 | generateHeader |
XDAS_Int32 | qValue |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IIMGENC1_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IIMGENC1_DynamicParams::numAU |
Number of Access unit to encode. Set to XDM_DEFAULT to encode the entire frame.
XDAS_Int32 IIMGENC1_DynamicParams::inputChromaFormat |
Input chroma format.
XDAS_Int32 IIMGENC1_DynamicParams::inputHeight |
Input frame height.
XDAS_Int32 IIMGENC1_DynamicParams::inputWidth |
Input frame width.
XDAS_Int32 IIMGENC1_DynamicParams::captureWidth |
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.
XDAS_Int32 IIMGENC1_DynamicParams::generateHeader |
Header generation mode.
XDAS_Int32 IIMGENC1_DynamicParams::qValue |
Quality factor for encoder. Set to a value between 0 (lowest quality) and 100 (highest quality).