![]() |
![]() |
XDAIS
dais-x04
|
Defines the creation time parameters for all IAUDDEC instance objects. More...
#include <iauddec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxSampleRate |
XDAS_Int32 | maxBitrate |
XDAS_Int32 | maxNoOfCh |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IAUDDEC_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC_Params::maxSampleRate |
Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.
XDAS_Int32 IAUDDEC_Params::maxBitrate |
Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.
XDAS_Int32 IAUDDEC_Params::maxNoOfCh |
Maximum Channels. See IAUDIO_ChannelId.
XDAS_Int32 IAUDDEC_Params::dataEndianness |
Endianness of input data.