![]() |
![]() |
XDAIS
dais-x04
|
Defines the input arguments for all IAUDDEC instance process function. More...
#include <iauddec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numBytes |
Defines the input arguments for all IAUDDEC instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IAUDDEC_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC_InArgs::numBytes |
Size of valid input data (in bytes) to be processed.