![]() |
![]() |
XDAIS
dais-x04
|
Data Structures | |
struct | IAUDENC_Obj |
This must be the first field of all IAUDENC instance objects. More... | |
struct | IAUDENC_Params |
Defines the creation time parameters for all IAUDENC instance objects. More... | |
struct | IAUDENC_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IAUDENC_InArgs |
Defines the input arguments for all IAUDENC instance process function. More... | |
struct | IAUDENC_Status |
Defines instance status parameters (read-only). More... | |
struct | IAUDENC_OutArgs |
Defines the run time output arguments for all IAUDENC instance objects. More... | |
struct | IAUDENC_Fxns |
Defines all of the operations on IAUDENC objects. More... |
Macros | |
#define | IAUDENC_CID "ti.xdais.dm.IAUDENC" |
#define | IAUDENC_ERUNTIME XDM_ERUNTIME |
#define | IAUDENC_EOK XDM_EOK |
| |
#define | IAUDENC_EFAIL XDM_EFAIL |
|
Typedefs | |
typedef struct IAUDENC_Obj | IAUDENC_Obj |
This must be the first field of all IAUDENC instance objects. | |
typedef struct IAUDENC_Obj * | IAUDENC_Handle |
Opaque handle to an IAUDENC objects. | |
typedef struct IAUDENC_Params | IAUDENC_Params |
Defines the creation time parameters for all IAUDENC instance objects. | |
typedef struct IAUDENC_DynamicParams | IAUDENC_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. | |
typedef struct IAUDENC_InArgs | IAUDENC_InArgs |
Defines the input arguments for all IAUDENC instance process function. | |
typedef struct IAUDENC_Status | IAUDENC_Status |
Defines instance status parameters (read-only). | |
typedef struct IAUDENC_OutArgs | IAUDENC_OutArgs |
Defines the run time output arguments for all IAUDENC instance objects. | |
typedef IALG_Cmd | IAUDENC_Cmd |
Defines the control commands for the IAUDENC module. | |
typedef struct IAUDENC_Fxns | IAUDENC_Fxns |
Defines all of the operations on IAUDENC objects. |
This is the XDM IAUDENC Audio Encoder Interface.
#define IAUDENC_CID "ti.xdais.dm.IAUDENC" |
IAUDENC Class ID
#define IAUDENC_ERUNTIME XDM_ERUNTIME |
General runtime failure.
#define IAUDENC_EOK XDM_EOK |
Success.
#define IAUDENC_EFAIL XDM_EFAIL |
General failure.
typedef struct IAUDENC_Obj IAUDENC_Obj |
This must be the first field of all IAUDENC instance objects.
typedef struct IAUDENC_Obj* IAUDENC_Handle |
Opaque handle to an IAUDENC objects.
typedef struct IAUDENC_Params IAUDENC_Params |
Defines the creation time parameters for all IAUDENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. typedef struct IAUDENC_DynamicParams IAUDENC_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IAUDENC_InArgs IAUDENC_InArgs |
Defines the input arguments for all IAUDENC instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IAUDENC_Status IAUDENC_Status |
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IAUDENC_OutArgs IAUDENC_OutArgs |
Defines the run time output arguments for all IAUDENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef IALG_Cmd IAUDENC_Cmd |
Defines the control commands for the IAUDENC module.
typedef struct IAUDENC_Fxns IAUDENC_Fxns |
Defines all of the operations on IAUDENC objects.