Defines the creation time parameters for all IVIDENC instance objects. More...
#include <ividenc.h>
Defines the creation time parameters for all IVIDENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Encoding preset.
Video rate control presets.
Maximum height.
Maximum width.
Maximum frame rate * 1000.
Maximum bit rate, bits per second.
Endianness of output data.
I to P frame distance. e.g. = 1 if no B frames, 2 to insert one B frame.
Chroma format for the input buffer.
Video content type of the buffer being encoded.