![]() |
![]() |
Defines the creation time parameters for all IAUDENC instance objects. More...
#include <iaudenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | encodingPreset |
XDAS_Int32 | maxSampleRate |
XDAS_Int32 | maxBitrate |
XDAS_Int32 | maxNoOfCh |
XDAS_Int32 | dataEndianness |
Defines the creation time parameters for all IAUDENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Encoding Preset. See XDM_EncodingPreset.
Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.
Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.
Maximum Channels. See IAUDIO_ChannelId.
Endianness of output data.