![]() |
![]() |
Defines instance status parameters (read-only). More...
#include <iaudenc1.h>
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Buffer descriptor for data passing.
Input and output buffer information.
Flag indicating the validity of the status struct.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Average bit rate, in bits per second.
Sampling frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Input Channel Mode.
Encoding mode.