Data Structures | |
struct | ISPHENC_Obj |
This must be the first field of all ISPHENC instance objects. More... | |
struct | ISPHENC_Params |
Defines the creation time parameters for all ISPHENC instance objects. More... | |
struct | ISPHENC_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. More... | |
struct | ISPHENC_InArgs |
Defines the input arguments for all ISPHENC instance process function. More... | |
struct | ISPHENC_Status |
Defines instance status parameters (read-only). More... | |
struct | ISPHENC_OutArgs |
Defines the run time output arguments for all ISPHENC instance objects. More... | |
struct | ISPHENC_Fxns |
Defines all of the operations on ISPHENC objects. More... | |
Defines | |
#define | ISPHENC_CID "ti.xdais.dm.ISPHENC" |
#define | ISPHENC_ERUNTIME XDM_ERUNTIME |
#define | ISPHENC_EOK XDM_EOK |
#define | ISPHENC_EFAIL XDM_EFAIL |
Typedefs | |
typedef struct ISPHENC_Obj | ISPHENC_Obj |
This must be the first field of all ISPHENC instance objects. | |
typedef struct ISPHENC_Obj * | ISPHENC_Handle |
Opaque handle to an ISPHENC objects. | |
typedef struct ISPHENC_Params | ISPHENC_Params |
Defines the creation time parameters for all ISPHENC instance objects. | |
typedef struct ISPHENC_DynamicParams | ISPHENC_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. | |
typedef struct ISPHENC_InArgs | ISPHENC_InArgs |
Defines the input arguments for all ISPHENC instance process function. | |
typedef struct ISPHENC_Status | ISPHENC_Status |
Defines instance status parameters (read-only). | |
typedef struct ISPHENC_OutArgs | ISPHENC_OutArgs |
Defines the run time output arguments for all ISPHENC instance objects. | |
typedef IALG_Cmd | ISPHENC_Cmd |
Defines the control commands for the ISPHENC module. | |
typedef struct ISPHENC_Fxns | ISPHENC_Fxns |
Defines all of the operations on ISPHENC objects. |
This is the XDM ISPHENC Speech/Voice Encoder Interface.
#define ISPHENC_CID "ti.xdais.dm.ISPHENC" |
ISPHENC Class ID
#define ISPHENC_ERUNTIME XDM_ERUNTIME |
General runtime failure.
#define ISPHENC_EOK XDM_EOK |
Success.
#define ISPHENC_EFAIL XDM_EFAIL |
General failure.
typedef struct ISPHENC_Obj ISPHENC_Obj |
This must be the first field of all ISPHENC instance objects.
typedef struct ISPHENC_Obj* ISPHENC_Handle |
Opaque handle to an ISPHENC objects.
typedef struct ISPHENC_Params ISPHENC_Params |
Defines the creation time parameters for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. typedef struct ISPHENC_DynamicParams ISPHENC_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct ISPHENC_InArgs ISPHENC_InArgs |
Defines the input arguments for all ISPHENC instance process function.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct ISPHENC_Status ISPHENC_Status |
Defines instance status parameters (read-only).
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef struct ISPHENC_OutArgs ISPHENC_OutArgs |
Defines the run time output arguments for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.typedef IALG_Cmd ISPHENC_Cmd |
Defines the control commands for the ISPHENC module.
typedef struct ISPHENC_Fxns ISPHENC_Fxns |
Defines all of the operations on ISPHENC objects.