Defines the creation time parameters for all IVIDTRANSCODE instance objects. More...
#include <ividtranscode.h>
Defines the creation time parameters for all IVIDTRANSCODE instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of output transcoded streams This allows the possibility of generating more than one transcoded bit-streams from a single incoming bit-stream.
Video Format types.
Video Format types.
Maximum video height in pixels.
Maximum video width in pixels.
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
Maximum output video height in pixels for each of the transcoded output.
Maximum output video width in pixels for each of the transcoded output.
Maximum frame rate in fps * 1000. for each out the output bitstreams For example, if max frame rate is 30 frames per second, set this field to 30000.
Maximum bit rate, in bits per second for each of the transcoded bitstreams. For example, if bit rate is 10 Mbps, set this field to 10000000
Endianness of output data.