Data Fields

IVIDTRANSCODE_OutArgs Struct Reference
[IVIDTRANSCODE - XDM Video Transcoder Interface]

Defines the run time output arguments for all IVIDTRANSCODE instance objects. More...

#include <ividtranscode.h>

Collaboration diagram for IVIDTRANSCODE_OutArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 bitsConsumed
XDAS_Int32 bitsGenerated [2]
XDAS_Int32 decodedPictureType
XDAS_Int32 decodedPictureStructure
XDAS_Int32 encodedPictureType [2]
XDAS_Int32 encodedPictureStructure [2]
XDAS_Int32 decodedHeight
XDAS_Int32 decodedWidth
XDAS_Int32 outputID [2]
XDAS_Int32 inputFrameSkipTranscodeFlag [2]
XDM1_SingleBufDesc encodedBuf [2]
XDAS_Int32 outBufsInUseFlag

Detailed Description

Defines the run time output arguments for all IVIDTRANSCODE instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDTRANSCODE_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
XDM_ErrorBit

Number of bits consumed during the IVIDTRANSCODE_Fxns.process() call.

Number of bits generated during the IVIDTRANSCODE_Fxns.process() call for each transcode output.

Type of the decoded picture.

See also:
IVIDEO_PictureType

Structure of the decoded picture.

See also:
IVIDEO_ContentType

Type of the encoded picture for each transcode output.

See also:
IVIDEO_PictureType

Structure of the encoded picture for each transcode output.

See also:
IVIDEO_ContentType

Decoded frame height

Decoded frame width

This is the ID of the encoded buffer for each output. This field is also used by the client to identify the outBufs supplied with the IVIDTRANSCODE_Fxns.process() call that can be reused.

Remarks:
This will be set to zero when there is no encoded buffer for passing to client application.
See also:
IVIDTRANSCODE_InArgs::inputID.

Flag to indicate if the current frame was skipped in specific transcode outputs.

Remarks:
Possible values XDAS_TRUE, XDAS_FALSE

When outputID for a specific transcode output is non-zero, the corresponding encoded buffer related information is populated here.

Flag to indicate that the outBufs provided with the IVIDTRANSCODE_Fxns.process() call are in use. No outBufs are required to be supplied with the next IVIDTRANSCODE_Fxns.process() call.

Remarks:
Possible values XDAS_TRUE, XDAS_FALSE

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated