Data Fields

IVIDDEC3_Status Struct Reference
[IVIDDEC3 - XDM Video Decoder Interface]

Defines instance status parameters. More...

#include <ividdec3.h>

Collaboration diagram for IVIDDEC3_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDM1_SingleBufDesc data
XDAS_Int32 maxNumDisplayBufs
XDAS_Int32 maxOutArgsDisplayBufs
XDAS_Int32 outputHeight
XDAS_Int32 outputWidth
XDAS_Int32 frameRate
XDAS_Int32 bitRate
XDAS_Int32 contentType
XDAS_Int32 sampleAspectRatioHeight
XDAS_Int32 sampleAspectRatioWidth
XDAS_Int32 bitRange
XDAS_Int32 forceChromaFormat
XDAS_Int32 operatingMode
XDAS_Int32 frameOrder
XDAS_Int32 inputDataMode
XDAS_Int32 outputDataMode
XDM1_AlgBufInfo bufInfo
XDAS_Int32 numInputDataUnits
XDAS_Int32 numOutputDataUnits
XDAS_Int32 configurationID
XDAS_Int32 metadataType [3]
IVIDDEC3_DynamicParams decDynamicParams

Detailed Description

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC3_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
XDM_ErrorBit

Buffer descriptor for data passing.

Remarks:
If this field is not used, the application must set data.buf to NULL.
This buffer can be used as either input or output, depending on the command.
The buffer will be provided by the application, and returned to the application upon return of the IVIDDEC3_Fxns.control() call. The algorithm must not retain a pointer to this data.
See also:
XDM_GETVERSION

The maximum number of buffers that will be required by the codec.

Remarks:
The maximum number of buffers can be IVIDEO2_MAX_IO_BUFFERS.

The maximum number of display buffers that can be returned via IVIDDEC3_OutArgs.displayBufs.

Remarks:
If returning display buffers embedded into the OutArgs struct, this field provides the size of the OutArgs.displayBufs.bufDesc[] array.

Output height in pixels.

Output width in pixels.

Average frame rate in fps * 1000. For example, if average frame rate is 30 frames per second, this field should be 30000.

Average bit rate, in bits per second.

Video content types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
IVIDEO_ContentType

Sample aspect ratio height.

Sample aspect ratio width.

Full 8 bit, CCIR 601

Output chroma format.

See also:
XDM_ChromaFormat

Video decoding mode of operation.

See also:
IVIDEO_OperatingMode

Frame Order

Remarks:
This field reflects the value provided during creation in IVIDDEC3_Params.displayDelay

Output data mode.

See also:
IVIDDEC3_Params.outputDataMode
IVIDEO_DataMode

Input and output buffer information.

Remarks:
This field provides the application with the algorithm's buffer requirements. The requirements may vary depending on the current configuration of the algorithm instance.
See also:
XDM1_AlgBufInfo

Number of input slices/rows.

Remarks:
Units depend on the IVIDDEC3_Params.inputDataMode, like number of slices/rows/blocks etc.
Ignored if IVIDDEC3_Params.inputDataMode is set to full frame mode.
See also:
IVIDDEC3_Params.inputDataMode

Number of output slices/rows.

Remarks:
Units depend on the outputDataMode, like number of slices/rows/blocks etc.
Ignored if IVIDDEC3_Params.outputDataMode is set to full frame mode.
See also:
IVIDDEC3_Params.outputDataMode

Configuration ID of given codec.

Remarks:
This is based on the input stream & can be used by the framework to optimize the save/restore overhead of any resources used.
This can be useful in multichannel use case scenarios.

Type of each metadata plane.

See also:
IVIDEO_MetadataType

Current values of the decoder's dynamic parameters.

Remarks:
This is the last field in the base struct as it can be extended.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated