Data Fields

IVIDANALYTICS_InArgs Struct Reference
[IVIDANALYTICS - XDM Beta Video Analytics Interface]

Defines the input arguments for all IVIDANALYTICS instance process function. More...

#include <ividanalytics.h>

Collaboration diagram for IVIDANALYTICS_InArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDM_Date date

Detailed Description

Defines the input arguments for all IVIDANALYTICS instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDANALYTICS_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Set the current time.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated