Data Fields

ISPHENC_DynamicParams Struct Reference
[ISPHENC - XDM Speech Encoder Interface]

This structure defines the codec parameters that can be modified after creation via control() calls. More...

#include <isphenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 frameSize
XDAS_Int32 bitRate
XDAS_Int32 mode
XDAS_Int32 vadFlag
XDAS_Int32 noiseSuppressionMode
XDAS_Int32 ttyTddMode
XDAS_Int32 dtmfMode
XDAS_Int32 dataTransmit
XDAS_Int32 homingMode

Detailed Description

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHENC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Input frame size in bytes for sample based codecs.

Rate selection for multi_rate codecs

Mode selection for multi_mode codecs

VAD_On =1, VAD_OFF = 0

0 - OFF, 1 = NS-A, 2 = NS-B etc

0 = TTY OFF, 1 = 45.45bauds 2 = 50 bauds

0 = DTMF_OFF, 1 = DTMF_ON

1 = ON, 0 = OFF

0 - DISABLED; 1 - ENABLED


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated