Defines the input arguments for all IIMGENC instance process() function. More...
#include <iimgenc.h>
Data Fields | |
XDAS_Int32 | size |
Defines the input arguments for all IIMGENC instance process() function.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.