![]() |
![]() |
Defines the run time output arguments for all IAUDDEC1 instance objects. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesConsumed |
XDAS_Int32 | numSamples |
XDAS_Int32 | channelMode |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | dualMonoMode |
XDAS_Int32 | sampleRate |
Defines the run time output arguments for all IAUDDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Number of bytes consumed during the process() call.
Number of output samples per channel.
Output Channel Configuration.
Flag indicating the precense of LFE channel in the output. When the LFE channel is not in the output, this is set to XDAS_FALSE.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Mode to indicate type of Dual Mono. Only used in case of Dual Mono output.
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.