IVIDENC1 - XDM Video Encoder Interface

Data Structures

struct  IVIDENC1_Obj
 This must be the first field of all IVIDENC1 instance objects. More...
struct  IVIDENC1_Params
 Defines the creation time parameters for all IVIDENC1 instance objects. More...
struct  IVIDENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IVIDENC1_InArgs
 Defines the input arguments for all IVIDENC1 instance process function. More...
struct  IVIDENC1_Status
 Defines instance status parameters. More...
struct  IVIDENC1_OutArgs
 Defines the run time output arguments for all IVIDENC1 instance objects. More...
struct  IVIDENC1_MbData
 Defines the structure that contains macroblock related encoding parameter estimates. More...
struct  IVIDENC1_Fxns
 Defines all of the operations on IVIDENC1 objects. More...

Defines

#define IVIDENC1_EOK   XDM_EOK
#define IVIDENC1_EFAIL   XDM_EFAIL
#define IVIDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IVIDENC1_ObjIVIDENC1_Handle
 Opaque handle to an IVIDENC1 objects.
typedef IALG_Cmd IVIDENC1_Cmd
 Defines the control commands for the IVIDENC1 module.

Detailed Description

This is the XDM IVIDENC1 Video Encoder Interface.


Define Documentation

#define IVIDENC1_EOK   XDM_EOK

Success.

#define IVIDENC1_EFAIL   XDM_EFAIL

General failure.

#define IVIDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IVIDENC1_Obj* IVIDENC1_Handle

Opaque handle to an IVIDENC1 objects.

Defines the control commands for the IVIDENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDENC1_Fxns::control()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated