IIMGENC1 - XDM Image Encoder Interface

Data Structures

struct  IIMGENC1_Obj
 This must be the first field of all IIMGENC1 instance objects. More...
struct  IIMGENC1_Params
 Defines the creation time parameters for all IIMGENC1 instance objects. More...
struct  IIMGENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IIMGENC1_InArgs
 Defines the input arguments for all IIMGENC1 instance process() function. More...
struct  IIMGENC1_Status
 Defines instance status parameters. More...
struct  IIMGENC1_OutArgs
 Defines the run time output arguments for all IIMGENC1 instance objects. More...
struct  IIMGENC1_Fxns
 Defines all of the operations on IIMGENC1 objects. More...

Defines

#define IIMGENC1_EOK   XDM_EOK
#define IIMGENC1_EFAIL   XDM_EFAIL
#define IIMGENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IIMGENC1_ObjIIMGENC1_Handle
 Opaque handle to an IIMGENC1 objects.
typedef IALG_Cmd IIMGENC1_Cmd
 Defines the control commands for the IIMGENC1 module.

Detailed Description

This is the XDM IIMGENC1 Image Encoder Interface.


Define Documentation

#define IIMGENC1_EOK   XDM_EOK

Success.

#define IIMGENC1_EFAIL   XDM_EFAIL

General failure.

#define IIMGENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IIMGENC1_Obj* IIMGENC1_Handle

Opaque handle to an IIMGENC1 objects.

Defines the control commands for the IIMGENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IIMGENC1_Fxns::control()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated